- Edited
jakaskerl
Thanks !
However, the behavior of the resize is still very strange to me. I just did a simple test:
- I used Luxonis Pro W, set resolution of Left camera at
THE_400_P
. - I didn't do any cropping, just simply resized to a random size, in this case i chose 480x640. I tested 2 types of resize: normal resize and resize with thumbnail. I received 2 different FoVs. You can see clearly that the FoV given by Normal resize is smaller than thumbnail resize (look at the right size of images, in the thumbnails you can see the image on the wall which doesnt appear in normal resize). That being said that your normal resize doesnt do only the resize but also other operations (crop maybe ?) ?
With normal resize
With thumbnail resize