@zdwiel I am very interested in your results. What FOV value did you find? I really need to know this in my case when using 4K resolution.
Zzdwiel
- Jun 4, 2022
- Joined Jun 3, 2022
- 0 best answers
@zdwiel
1) The software sync for the camera modules within one device (rgb, left, right) happens automatically. The mechanism is explained here:
https://docs.luxonis.com/projects/hardware/en/latest/pages/guides/sync_frames.html?#software-soft-syncSoftware “soft” sync
Through firmware sync, we’re monitoring for drift and aligning the capture timestamps of the cameras, which are taken at the MIPI Start-of-Frame event. The Left/Right global shutter cameras are driven by the same clock, started by broadcast write on I2C, so no drift will happen over time, even when running freely without a sync. With the above functionality it would be also possible to configure FSIN as an output on one sensor, and an input to the other sensor. The RGB rolling shutter has a slight difference in clocking/frame-time, so when we detect a small drift, we’re modifying the frame time (number of lines) for the next frame by a small amount to compensate.
All 3 cameras are soft-synced by default using the above method, as long as they are configured with the same FPS (default is 30).
For multiple devices, currently we don't have a way to do soft sync.
host-multiple-OAK-sync.py
is actually just matching frames on host as close as possible based on their timestamps.
But we were thinking to implement a soft sync mechanism for multiple devices connected to the same host as: a time-sync mechanism already runs in the background, and all devices are aware of the host time. Two options from here:- each device will try to align the capture time for its RGB/L/R cameras at host time intervals multiple of a period, based on the configured FPS. For example for an FPS of 20, the interval would be 50ms, and the devices will try to align the capture at host timestamps like: 1000.2s, 1000.25s, 1000.3s, ...
- the host could monitor the frame timestamps from each device, and decide to issue frame-time adjustment commands (+/- a small time interval) for cameras that are drifting, that would be applied once (one frame-time is corrected, then the camera goes back to its configured frame-time -- based on FPS).
2) As you said, capturing the stopwatch shown on the monitor isn't a good way to measure how good the sync is, it was added just to show that the frames captured are actually in sync, and not far apart by a large number. For each camera, we do capture a timestamp on device and attach it as metadata to the
ImgFrame
object. You can check the timestamp diff between cameras as here:
https://github.com/luxonis/depthai-experiments/blob/master/gen2-syncing/README.md#output-with-logging-enabledSeq Left_tstamp RGB-Left Right-Left Dropped num [seconds] diff[ms] diff[ms] delta 0 0.055592 -0.785 0.017 1 0.088907 -0.771 0.011 2 0.122222 -0.758 0.009 3 0.155537 -0.745 0.010 4 0.188852 -0.340 0.011 5 0.222167 -0.326 0.011 6 0.255482 0.063 0.010 7 0.288796 0.078 0.010 8 0.322111 0.257 0.010 9 0.355426 0.270 0.009 10 0.388741 0.246 0.010 11 0.422056 0.260 0.011 12 0.455371 0.146 0.009 13 0.488686 0.160 0.009 14 0.522000 0.046 0.010 15 0.555315 0.061 0.010 16 0.588644 -0.015 0.010 17 0.621945 0.020 0.011 18 0.655267 -0.011 0.008 19 0.688575 0.019 0.010 20 0.721890 0.018 0.009 ...