Z
zdwiel

  • Jun 4, 2022
  • Joined Jun 3, 2022
  • 0 best answers
  • Brandon the link above is broken. Here is the updated link: https://github.com/luxonis/depthai-experiments/tree/master/gen2-syncing

    Also, a couple questions:

    1) is there anything in that code example that is causing software sync? Does it happen automatically?
    2) How accurate can I expect software sync to be? The pictures in that demo show time resolution of milliseconds, but I assume your monitor isn't refreshing at 1000 FPS so accuracy of this measurement isn't actually to the millisecond. It seems the monitor is likely running at 60fps or 120fps which means that we can trust the devices are in sync to within 16 ms or 8 ms. Do you have any more precise data on just how close the multi-device synchronization is?

    Thanks