SDV

- Jul 30, 2024
- Joined Sep 12, 2023
- 0 best answers
- Edited
I've made others tests and I found something odd.
These are timestamps taken using 15Hz acquisition frequency:
Timestamp (ms) Delta t (ms)
0 0
59,922 59,922
119,826 59,904
179,751 59,925
239,489 59,738
299,436 59,947
359,638 60,202
419,441 59,803All intervals are around 60 ms but at 15 Hz, it should be 66 ms
if there are 6 ms of error on 66 then there is a 10% of error.
Is it possible that for some reason the interval reported is shorter than the real?
I've made many other try changing the way dt is evaluate, using acceleroValues.getTimestamp()
but values are totally unreliable leading to very high speed or negative speed
- Edited
As you can see there i negative speed while the camere nevere move backward
I suspect that the camera timestamp is not correct.
`Hi. Im using this code:
#!/usr/bin/env python3
import cv2
import depthai as dai
import time
import numpy as np
import csv
# Create pipeline
pipeline = dai.Pipeline()
# Define sources and outputs
imu = pipeline.create(dai.node.IMU)
xlinkOut = pipeline.create(dai.node.XLinkOut)
xlinkOut.setStreamName("imu")
# enable ACCELEROMETER_RAW at 500 hz rate
imu.enableIMUSensor(dai.IMUSensor.LINEAR_ACCELERATION, 500)
# enable GYROSCOPE_RAW at 400 hz rate
imu.enableIMUSensor(dai.IMUSensor.GYROSCOPE_CALIBRATED, 400)
# it's recommended to set both setBatchReportThreshold and setMaxBatchReports to 20 when integrating in a pipeline with a lot of input/output connections
# above this threshold packets will be sent in batch of X, if the host is not blocked and USB bandwidth is available
imu.setBatchReportThreshold(1)
# maximum number of IMU packets in a batch, if it's reached device will block sending until host can receive it
# if lower or equal to batchReportThreshold then the sending is always blocking on device
# useful to reduce device's CPU load and number of lost packets, if CPU load is high on device side due to multiple nodes
imu.setMaxBatchReports(10)
# Link plugins IMU -> XLINK
imu.out.link(xlinkOut.input)
# Function to write data to CSV
def write_to_csv(data, filename='imu_data.csv'):
with open(filename, mode='a', newline='') as file: writer = csv.writer(file) writer.writerow(data)
# Write CSV header
write_to_csv(['Timestamp (ms)', 'Delta t (ms)', 'Accel X (m/s2)', 'Accel Y (m/s2)', 'Accel Z (m/s2)', 'Velocity X (km/h)', 'Velocity Y (km/h)', 'Velocity Z (km/h)'])
# Pipeline is defined, now we can connect to the device
with dai.Device(pipeline) as device:
def timeDeltaToMilliS(delta) -> float: return delta.total_seconds() \* 1000 # Output queue for imu bulk packets imuQueue = device.getOutputQueue(name="imu", maxSize=50, blocking=False) baseTs = None velocity = np.array([0.0, 0.0, 0.0]) lastTs = None while True: imuData = imuQueue.get() # blocking call, will wait until new data has arrived imuPackets = imuData.packets for imuPacket in imuPackets: acceleroValues = imuPacket.acceleroMeter acceleroTs = acceleroValues.getTimestampDevice() if baseTs is None: baseTs = acceleroTs acceleroTs = timeDeltaToMilliS(acceleroTs - baseTs) # Calculate time difference currentTs = acceleroTs / 1000.0 # convert to seconds if lastTs is not None: dt = currentTs - lastTs # Read acceleration acceleration = np.array([acceleroValues.x, acceleroValues.y, acceleroValues.z]) # Integrate acceleration to get velocity velocity += acceleration \* dt # Convert velocity to km/h velocity_kmh = velocity \* 3.6 imuF = "{:.1f}" print(f"Delta t: {imuF.format(dt \* 1000)} ms") print(f"Accelerometer [m/s^2]: x: {imuF.format(acceleroValues.x)} y: {imuF.format(acceleroValues.y)} z: {imuF.format(acceleroValues.z)}") print(f"Velocity [km/h]: x: {imuF.format(velocity_kmh[0])} y: {imuF.format(velocity_kmh[1])} z: {imuF.format(velocity_kmh[2])}") # Write data to CSV write_to_csv([currentTs \* 1000, dt \* 1000, acceleroValues.x, acceleroValues.y, acceleroValues.z, velocity_kmh[0], velocity_kmh[1], velocity_kmh[2]]) lastTs = currentTs if cv2.waitKey(1) == ord('q'): break\`
And this is part of the data collected:
Timestamp (ms),Delta t (ms),Accel X (m/s2),Accel Y (m/s2),Accel Z (m/s2),Velocity X (km/h),Velocity Y (km/h),Velocity Z (km/h)
7.3629999999999995,7.3629999999999995,1.41015625,0.0234375,-0.0625,0.037378729687499994,0.0006212531249999999,-0.001656675
9.718,2.3549999999999995,1.453125,0.015625,-0.44140625,0.0496983234375,0.0007537218749999999,-0.005398917187499999
12.235,2.5170000000000003,0.42578125,-0.21484375,-0.609375,0.0535564125,-0.0011930203125000002,-0.0109205859375
14.815999999999999,2.581,0.31640625,-0.19921875,-0.546875,0.0564963328125,-0.00304408125,-0.0160019296875
17.194999999999997,2.3789999999999956,-1.046875,-0.09765625,-0.87890625,0.047530476562500014,-0.0038804484374999984,-0.02352923437499999
19.754,2.5590000000000055,-1.5625,0.015625,0.18359375,0.033136101562499985,-0.003736504687499998,-0.021837895312499984
22.226,2.4719999999999986,-1.4921875,0.0234375,0.19921875,0.019856826562499992,-0.003527929687499998,-0.020065007812499983
24.621000000000002,2.3950000000000014,-1.2734375,0.04296875,0.1015625,0.008877248437499987,-0.003157453124999998,-0.019189335937499982
28.909,4.287999999999997,0.27734375,-0.0859375,0.58203125,0.013158548437499985,-0.0044840531249999965,-0.010204635937499991
31.405,2.4960000000000053,1.203125,0.1171875,-0.1796875,0.023969348437500006,-0.003431053124999994,-0.011819235937499993
37.138999999999996,5.733999999999996,1.52734375,0.10546875,-0.29296875,0.05549738906249998,-0.0012539249999999958,-0.017866814062499993
54.576,17.437,-1.12109375,0.078125,0.0,-0.014877253125000026,0.003650231250000005,-0.017866814062499993
64.731,10.154999999999998,1.28125,0.109375,0.05859375,0.03196268437499997,0.007648762500000004,-0.015724743749999992
78.067,13.336,-0.9453125,0.07421875,0.2109375,-0.013421390625000034,0.011211975000000004,-0.005597718749999991
89.89800000000001,11.831000000000008,1.26171875,-0.01953125,-0.19140625,0.040317229687500004,0.010380107812500003,-0.013750017187499996
99.652,9.754,-1.20703125,-0.0390625,-0.03125,-0.002066948437499989,0.009008451562500004,-0.014847342187499998
113.319,13.666999999999998,1.5625,0.09375,-0.30078125,0.0748099265625,0.013621064062500002,-0.029646140624999994
121.965,8.646,-0.33984375,-0.14453125,-0.6640625,0.0642320859375,0.009122442187500003,-0.050315484375
129.46699999999998,7.501999999999967,-1.515625,0.0859375,-0.04296875,0.023299298437500178,0.011443373437499993,-0.05147594999999999
136.97799999999998,7.511000000000018,1.0859375,0.06640625,0.33984375,0.05266261406250025,0.013238971874999996,-0.042286710937499965
144.459,7.481000000000016,0.73046875,-0.0078125,-0.06640625,0.0723353062500003,0.013028568749999997,-0.044075137499999965
160.09,15.631000000000006,-0.0234375,-0.046875,0.62109375,0.0710164406250003,0.010390837499999996,-0.009125198437499954
171.66400000000002,11.574000000000002,0.578125,-0.19921875,-0.3125,0.09510482812500029,0.0020901093749999943,-0.022145948437499955
179.61599999999999,7.951999999999987,-1.48046875,0.01171875,0.1640625,0.05272315312500036,0.002425584374999994,-0.017449298437499962
191.409,11.792999999999997,1.421875,0.05859375,0.01953125,0.11308857187500036,0.0049131703124999935,-0.016620103124999966
192.086,0.6770000000000109,1.421875,0.05859375,0.01953125,0.11655396562500041,0.005055974999999995,-0.016572501562499963
209.376,17.29,-1.48828125,0.01171875,0.2578125,0.02391738750000041,0.005785396874999994,-0.0005252203124999636
221.906,12.529999999999985,1.55859375,0.13671875,0.0546875,0.09422243437500033,0.011952506249999988,0.0019416234375000336
238.209,16.30300000000001,-0.78125,0.05859375,0.16015625,0.0483702468750003,0.01539142031249999,0.011341321875000039
256.839,18.62999999999998,-0.38671875,-0.16015625,-0.58984375,0.022433793750000323,0.004650060937500002,-0.02821831874999992
274.304,17.465000000000007,1.81640625,0.05859375,-0.17578125,0.1366385203125004,0.008334084375000004,-0.039270389062499925
289.566,15.261999999999997,-1.44921875,0.05859375,-0.0625,0.05701380468750041,0.011553412500000002,-0.04270433906249993
296.78900000000004,7.2230000000000345,1.3671875,0.046875,0.1875,0.0925645078125006,0.012772293750000009,-0.0378288140624999
316.753,19.96399999999998,-1.3359375,0.09765625,0.1015625,-0.003449854687499325,0.019790887500000003,-0.03052947656249991
339.51,22.756999999999973,-1.8515625,0.01953125,0.2734375,-0.15513948281249915,0.0213909890625,-0.008128054687499938
359.321,19.81100000000002,-0.47265625,-0.2109375,0.1015625,-0.18884913749999918,0.006347010937499982,-0.0008846578124999297
374.20799999999997,14.886999999999983,-0.23046875,0.046875,-0.234375,-0.20120069531249915,0.00885919218749998,-0.013445564062499917
379.108,4.9000000000000155,2.09375,0.078125,0.1484375,-0.16426694531249902,0.010237317187499984,-0.010827126562499907
386.581,7.473000000000008,-1.0,-0.02734375,0.3984375,-0.19116974531249906,0.009501693749999984,-0.0001080421874998969
403.961,17.380000000000006,2.1875,0.02734375,-0.81640625,-0.05430224531249899,0.011212537499999986,-0.051188948437499916
421.554,17.592999999999968,-1.36328125,0.0546875,0.9453125,-0.14064539062499884,0.01467615937499998,0.008682229687499975
439.448,17.89400000000002,-1.48828125,-0.05859375,-0.0625,-0.23651808749999897,0.010901643749999976,0.00465607968749997
452.866,13.417999999999985,3.04296875,0.171875,-1.26953125,-0.08952809062499911,0.01920403124999997,-0.05666837343749997
468.518,15.652,-1.39453125,0.15234375,0.42578125,-0.16810602187499912,0.027788174999999967,-0.03267679218749996
476.21599999999995,7.697999999999983,2.58203125,0.21875,-0.96875,-0.09655070624999929,0.03385034999999996,-0.059523567187499904
494.28,18.064000000000025,-2.140625,0.14453125,1.81640625,-0.23575640624999947,0.04324927499999997,0.05859805781250026
503.908,9.628000000000025,3.078125,0.11328125,-1.515625,-0.1290661312499992,0.047175693749999977,0.006065282812500121
511.344,7.435999999999998,-1.74609375,-0.23046875,-0.88671875,-0.17580836249999918,0.04100613749999998,-0.017671823437499873
531.3919999999999,20.047999999999956,1.65625,-0.01171875,-1.0078125,-0.056272162499999424,0.040160362499999984,-0.0904084734374997
597.305,65.913,0.30078125,0.10546875,-0.46484375,0.01509925781250057,0.06518670468749999,-0.2007097593749997
647.981,50.67600000000005,0.609375,0.0078125,-0.75390625,0.12626973281250067,0.06661196718749998,-0.33824759062499987
658.712,10.730999999999934,2.015625,-0.3671875,-2.0390625,0.2041365515625002,0.052426926562500066,-0.4170198374999994
673.918,15.206000000000053,-0.58984375,0.0625,-0.171875,0.17184756093750012,0.05584827656250008,-0.4264285499999994
694.723,20.804999999999964,-0.58984375,0.15234375,2.76171875,0.1276694437500002,0.06725851875000005,-0.21958133906249977
711.073,16.349999999999977,-1.5,-0.328125,-0.9453125,0.03937944375000033,0.047945081250000084,-0.27522243281249975
723.533,12.460000000000026,-0.03125,0.15234375,-0.41796875,0.03797769375000033,0.0547786125000001,-0.29397083906249977
733.524,9.990999999999971,2.96484375,0.0859375,-1.9453125,0.14461600781250003,0.05786957812500009,-0.3639390609374996
746.26,12.73600000000008,-1.3359375,0.2578125,0.39453125,0.08336380781249964,0.06969017812500017,-0.3458499609374995
753.544,7.283999999999957,2.734375,-0.0390625,-1.2734375,0.15506568281249922,0.06866586562500018,-0.3792425484374993
760.985,7.441000000000031,1.91796875,-0.14453125,0.36328125,0.20644346249999942,0.06479422031250016,-0.3695111156249993
772.745,11.759999999999993,0.2890625,0.08203125,-0.0859375,0.21868121249999942,0.06826709531250016,-0.3731493656249993
778.3919999999999,5.646999999999958,1.8984375,0.015625,-1.0,0.25727492812499914,0.06858473906250015,-0.3934785656249991
795.9209999999999,17.529000000000018,-3.234375,0.1015625,0.79296875,0.05317163437499892,0.07499377968750016,-0.34343874843749905
807.79,11.869000000000018,1.8359375,-0.203125,1.03125,0.13161830624999907,0.06631457343750015,-0.299375085937499
819.5519999999999,11.76199999999994,-2.48828125,0.09375,0.46484375,0.026256515624999605,0.07028424843750013,-0.27969211406249916
843.433,23.881000000000043,-3.05078125,0.12109375,0.75390625,-0.23602402968750083,0.08069487187500014,-0.21487758749999902
850.829,7.395999999999958,1.10546875,-0.078125,-0.203125,-0.20659026093750102,0.07861474687500015,-0.22028591249999901
858.428,7.599000000000022,1.98828125,-0.21484375,1.10546875,-0.15219804375000084,0.07273739531250013,-0.19004426718749892
878.398,19.97000000000004,1.484375,0.02734375,-0.76171875,-0.04548335625000062,0.07470319218750014,-0.24480575156249904
886.02,7.622000000000018,-0.078125,-0.26953125,-1.22265625,-0.047627043750000625,0.06730747031250012,-0.27835446093749916
903.433,17.41300000000001,1.140625,-0.0234375,-0.13671875,0.02387508749999942,0.06583824843750011,-0.28692492187499913
920.848,17.414999999999957,-1.67578125,0.10546875,3.40234375,-0.08118634218750033,0.0724505062500001,-0.07361838281249965
936.812,15.963999999999977,-0.171875,-0.0390625,-0.90625,-0.09106406718750032,0.0702055687500001,-0.12570093281249958
955.748,18.936000000000064,0.875,0.0,-0.08203125,-0.03141566718750012,0.0702055687500001,-0.13129297031249962
963.6289999999999,7.880999999999916,1.66015625,-0.26953125,-0.76171875,0.01568562187499938,0.06255853593750019,-0.15290414999999938
975.7679999999999,12.13900000000001,-0.28515625,0.046875,0.01953125,0.0032241796874993662,0.0646069921875002,-0.15205062656249937
991.317,15.549000000000035,-1.609375,0.046875,-0.9296875,-0.08686283906250084,0.0672308859375002,-0.20409118593749948
1015.6400000000001,24.323000000000093,0.22265625,0.0078125,0.71875,-0.06736643437500077,0.0679149703125002,-0.14115542343749923
1034.039,18.39899999999983,2.453125,0.0,-1.76953125,0.09511973437499774,0.0679149703125002,-0.25836280312499815
1043.08,9.041000000000077,-1.359375,-0.10546875,-0.78515625,0.05087534062499737,0.06448221562500017,-0.2839177546874984
1053.598,10.518000000000027,0.8046875,-0.01171875,1.19921875,0.08134467187499744,0.06403848750000017,-0.23850957656249827
1060.4560000000001,6.858000000000031,2.828125,-0.01171875,0.5,0.15116768437499775,0.06374916562500017,-0.2261651765624982
1069.37,8.913999999999866,-2.01953125,-0.125,-0.046875,0.08636011874999872,0.05973786562500023,-0.2276694140624982
1078.0590000000002,8.689000000000169,-0.859375,0.3515625,0.328125,0.05947852499999819,0.07073488125000044,-0.21740553281249797
1100.688,22.629000000000012,-1.37890625,0.19921875,1.41796875,-0.052853245312501865,0.08696411718750044,-0.10189155937499791
1116.377,15.688999999999842,-0.34765625,-0.2578125,-0.765625,-0.07248900937500168,0.0724027640625006,-0.14513436562499749
1122.9530000000002,6.576000000000359,-2.0859375,-0.01171875,-0.515625,-0.12187065937500438,0.07212533906250058,-0.15734106562499817
1133.193,10.239999999999583,1.33984375,-0.078125,0.8671875,-0.0724786593750064,0.0692453390625007,-0.12537306562499947
1147.934,14.741000000000115,-2.5078125,0.0078125,0.77734375,-0.20556225000000744,0.0696599296875007,-0.08412129843749913
1157.883,9.948999999999986,0.10546875,0.07421875,0.03125,-0.20178473906250743,0.0723181781250007,-0.08300203593749914
1167.249,9.365999999999985,0.1796875,-0.1953125,-0.77734375,-0.19572610781250743,0.06573270937500071,-0.1092122015624991
1180.39,13.14100000000007,-0.421875,0.21875,1.40625,-0.21568400156250755,0.07608124687500077,-0.04268588906249875
1197.7930000000001,17.403000000000056,-1.0546875,-0.15234375,-0.11328125,-0.2817610171875078,0.06653678906250073,-0.04978304999999877
1217.501,19.707999999999835,-0.21875,-0.14453125,-0.66015625,-0.2972810671875077,0.05628247031250082,-0.09662034374999838
1232.778,15.276999999999985,-0.40234375,0.16015625,1.1953125,-0.31940884687500765,0.06509061562500082,-0.030881503124998433
1245.1970000000001,12.41900000000018,-1.015625,-0.2421875,0.36328125,-0.3648158156250083,0.05426280000000065,-0.014639779687498198
1262.575,17.377999999999894,2.14453125,0.0625,-1.00390625,-0.23065222500000915,0.05817285000000064,-0.07744495781249781
1272.086,9.511000000000047,-1.9453125,-0.00390625,-0.515625,-0.2972589468750095,0.05803910156250064,-0.0950997515624979
1285.155,13.068999999999997,1.1875,-0.00390625,0.69140625,-0.24138897187500946,0.05785531875000064,-0.06257019374999791
1295.698,10.542999999999969,-0.8515625,-0.12890625,0.390625,-0.2737098562500094,0.052962707812500655,-0.04774409999999795
1311.107,15.409000000000006,2.0390625,0.04296875,-0.91796875,-0.1605981656250093,0.05534628750000065,-0.09866602968749798
1322.545,11.43800000000006,0.18359375,-0.30859375,-0.796875,-0.15303836250000927,0.04263938437500059,-0.13147879218749814
1332.675,10.129999999999972,-0.44140625,0.1484375,1.78125,-0.16913556562500923,0.04805260312500057,-0.06652016718749831
1346.958,14.283000000000046,-0.9765625,-0.2890625,0.1640625,-0.2193492375000094,0.03318935625000053,-0.058084270312498285
1357.845,10.886999999999869,-2.0703125,0.29296875,0.69921875,-0.3004914093750084,0.04467173906250039,-0.030679649999998615
1373.612,15.767000000000087,-2.1953125,-0.0234375,-0.7578125,-0.4250999812500091,0.04334139843750038,-0.07369399687499885
1382.679,9.066999999999936,-1.07421875,0.25390625,0.3671875,-0.4601637703125088,0.05162920312500032,-0.061708556249998936
1393.0739999999998,10.394999999999932,2.11328125,-0.015625,0.32421875,-0.38108055937500934,0.05104448437500033,-0.04957564218749901
1402.414,9.340000000000126,-2.30859375,0.109375,0.66796875,-0.4587047156250104,0.054722109375000376,-0.027115860937498713
1420.389,17.974999999999852,0.3125,-0.29296875,-1.03515625,-0.4384828406250106,0.03576410156250053,-0.09410082187499816
1440.01,19.62100000000011,3.45703125,0.1015625,-1.4765625,-0.19429336406250922,0.04293802968750057,-0.19839869999999876
1444.884,4.874000000000045,2.0,-0.13671875,-0.91015625,-0.1592005640625089,0.04053910781250055,-0.21436866562499893
1467.433,22.54899999999993,2.9375,0.03515625,-1.88671875,0.07925511093749038,0.04339296562500054,-0.3675257015624985
1475.497,8.064000000000071,-2.08984375,0.03515625,-0.76953125,0.018586110937489842,0.04441356562500055,-0.38986550156249866
1498.54,23.042999999999925,-0.328125,-0.1015625,1.68359375,-0.008633432812510071,0.035988468750000585,-0.2502033187499991
1514.921,16.38099999999998,1.73046875,0.0625,-1.19140625,0.0934150781249898,0.03967419375000058,-0.32046245156249903
1533.6860000000001,18.765000000000143,-1.53515625,0.1953125,0.16796875,-0.010290867187510992,0.05286833437500068,-0.30911549062499893
1556.975,23.288999999999895,-1.92578125,0.1484375,2.87890625,-0.17174913750001025,0.06531339375000063,-0.06774683906250005
1562.229,5.254000000000092,0.3515625,0.01171875,0.265625,-0.16509954375001012,0.06553504687500064,-0.06272270156249997
1572.1719999999998,9.942999999999813,2.75390625,0.12109375,-1.8984375,-0.06652402031251199,0.06986957343750055,-0.1306768921874987
1584.6180000000002,12.44600000000018,-1.7578125,0.41796875,0.1796875,-0.14528386406251315,0.08859691406250082,-0.1226258859374986
1599.672,15.0539999999999,2.1796875,0.1015625,-1.2109375,-0.027157007812513914,0.09410103281250079,-0.18825191718749817
1617.299,17.62700000000006,1.5703125,0.0234375,-0.328125,0.07249062656248642,0.0955883109375008,-0.20907381093749824
1627.2949999999998,9.995999999999894,-1.171875,-0.03515625,-0.90625,0.03032000156248687,0.0943231921875008,-0.2416857609374979
1646.695,19.400000000000084,2.62109375,0.04296875,-1.65234375,0.21337718906248768,0.09732412968750082,-0.3570854484374984
1666.4730000000002,19.778000000000073,0.65625,0.05078125,-0.0546875,0.26010271406248786,0.10093979531250083,-0.3609792421874984
1679.519,13.045999999999891,-0.28125,-0.03515625,-0.80078125,0.24689363906248799,0.09928866093750084,-0.3985884140624981
1699.598,20.078999999999958,2.6015625,0.078125,-1.3046875,0.43494602343748756,0.10493587968750083,-0.4928969671874979
1722.182,22.58400000000016,1.40234375,0.0625,-0.67578125,0.5489599359374884,0.11001727968750087,-0.5478396046874984
1754.434,32.251999999999946,1.7265625,0.0390625,-0.80078125,0.749426273437488,0.11455271718750087,-0.6408160734374981
1766.987,12.553000000000036,-2.140625,0.05078125,0.453125,0.6526897171874877,0.11684756250000088,-0.6203389921874981
1792.265,25.277999999999913,-2.19921875,0.109375,0.109375,0.4525590515624885,0.12680077500000084,-0.6103857796874982
1810.617,18.351999999999926,-0.59765625,-0.140625,-0.5625,0.41307357656248866,0.11751007500000087,-0.647548579687498
1829.9959999999999,19.379000000000033,1.49609375,0.0859375,-0.6875,0.5174476593749888,0.12350545312500087,-0.6955116046874982
1845.65,15.654000000000057,-1.7578125,0.0703125,-0.16015625,0.41838719062498847,0.1274678718750009,-0.7045371140624982
1861.674,16.024000000000036,0.53125,-0.0546875,-0.3515625,0.4490330906249886,0.12431314687500086,-0.7248174890624982
1876.757,15.082999999999958,-1.5,0.03125,-0.1796875,0.36758489062498884,0.12600998437500086,-0.7345743046874983
1892.618,15.860999999999903,-0.46484375,-0.12109375,-0.59375,0.34104249843748896,0.1190955796875009,-0.768477192187498
1896.993,4.375000000000018,-1.38671875,-0.07421875,-0.14453125,0.3192016781249889,0.11792663437500088,-0.770753559374998
1916.786,19.79300000000017,0.3125,-0.10546875,-0.37109375,0.34146880312498906,0.11041147968750081,-0.7971957703124982
1931.846,15.059999999999851,-0.140625,0.10546875,-0.02734375,0.33384467812498914,0.11612957343750076,-0.7986782390624984
1946.961,15.11499999999999,-0.6015625,-0.03515625,-0.515625,0.30111125624998913,0.11421658125000075,-0.8267354578124982
1964.143,17.18200000000003,0.94921875,0.17578125,-0.53515625,0.3598253718749893,0.1250895656250008,-0.8598376546874983
1971.6149999999998,7.471999999999701,0.26953125,-0.12109375,-0.44921875,0.367075546874989,0.1218322406250009,-0.8719212796874978
1982.586,10.971000000000286,-0.83984375,0.0703125,0.18359375,0.33390541406248814,0.12460927500000099,-0.8646701343749976
1998.955,16.369000000000078,0.109375,0.04296875,-0.4296875,0.34035070781248816,0.127141354687501,-0.8899909312499977
2016.616,17.660999999999927,0.03125,0.125,-0.01953125,0.3423375703124882,0.13508880468750098,-0.8912327203124977
2036.8439999999998,20.227999999999913,-0.80078125,0.0703125,0.06640625,0.28402403906248846,0.14020901718750095,-0.8863969640624977
2045.554,8.710000000000218,1.5625,0.1171875,-0.5,0.3330177890624897,0.14388354843750104,-0.9020749640624981
2058.967,13.412999999999897,-1.26953125,0.03125,-0.15625,0.27171618749999016,0.14539251093750102,-0.909619776562498
2065.516,6.549000000000138,-0.640625,0.10546875,0.171875,0.25661255624998985,0.14787908437500108,-0.9055675828124979
2071.93,6.41399999999992,1.67578125,0.14453125,-0.296875,0.2953070156249894,0.15121636875000102,-0.9124225453124978
2087.487,15.556999999999821,-1.6953125,0.15625,-0.01953125,0.20036069999999048,0.15996718125000092,-0.9135163968749979
2101.441,13.954000000000022,1.92578125,0.078125,-0.23828125,0.29710116562499067,0.16389174375000093,-0.925486312499998
2107.1240000000003,5.683000000000327,-0.2578125,0.03125,-0.25,0.2918266312499903,0.16453108125000096,-0.9306010124999983
2116.452,9.328000000000003,-1.875,0.10546875,0.11328125,0.22886263124999032,0.16807280625000098,-0.9267969374999984
2126.406,9.953999999999574,0.90234375,0.13671875,-0.3828125,0.2611975781249889,0.17297204062500074,-0.9405147937499978
2141.299,14.893000000000267,-1.5703125,0.0859375,0.20703125,0.17700558749998738,0.17757956250000081,-0.9294148546874976
2158.757,17.457999999999974,0.40234375,-0.0859375,-0.375,0.20229240937498735,0.17217849375000083,-0.9529831546874976
2171.176,12.418999999999958,-0.765625,0.05859375,0.24609375,0.16806254062498746,0.17479812656250082,-0.9419806968749975
2188.824,17.647999999999886,-0.0546875,0.03125,0.0546875,0.16458809062498747,0.1767835265625008,-0.9385062468749975
2205.342,16.518000000000033,1.4375,0.15625,-0.328125,0.25006874062498763,0.1860749015625008,-0.9580181343749975
2224.0820000000003,18.7400000000002,-0.5546875,0.0625,0.265625,0.21264730312498725,0.19029140156250085,-0.9400980093749973
2238.698,14.61599999999974,1.1015625,0.03125,0.390625,0.2706088781249862,0.19193570156250084,-0.9195442593749976
2256.198,17.50000000000007,0.6328125,0.1171875,-0.05078125,0.31047606562498636,0.19931851406250087,-0.9227434781249977
2263.675,7.477000000000178,1.29296875,0.05859375,0.4765625,0.3452791640624872,0.2008956937500009,-0.9099157499999974
2271.065,7.390000000000008,-1.0078125,-0.046875,-0.203125,0.31846732031248715,0.1996486312500009,-0.9153196874999974
2283.5519999999997,12.486999999999693,0.51953125,0.0703125,0.046875,0.34182191249998656,0.20280940312500084,-0.9132125062499974
2294.441,10.889000000000149,0.06640625,-0.12109375,-0.3203125,0.3444250640624866,0.1980624796875008,-0.9257688843749976
2301.168,6.7270000000001495,-0.98828125,-0.12109375,-0.08984375,0.320491659374986,0.1951299281250007,-0.9279446484374977
2308.8540000000003,7.686000000000082,-0.23828125,0.05859375,0.03515625,0.31389851249998596,0.19675119375000075,-0.9269718890624977
2326.245,17.39099999999949,-1.11328125,-0.0546875,0.07421875,0.24419864531248803,0.19332734062500084,-0.9223252312499978
2338.503,12.258000000000546,0.8515625,-0.0546875,0.640625,0.28177707656248974,0.19091404687500074,-0.8940552187499965
2355.971,17.467999999999595,-0.74609375,-0.02734375,-0.1640625,0.23485912031249082,0.1891945406250008,-0.9043722562499963
2373.526,17.55500000000021,0.94921875,-0.07421875,-0.26171875,0.29484784687499155,0.18450406406250072,-0.9209123578124966
2391.997,18.470999999999904,0.9296875,0.078125,0.54296875,0.3566679749999912,0.1896990328125007,-0.8848073249999967
2407.4840000000004,15.48700000000025,-1.16015625,0.0703125,0.2265625,0.2919855515624902,0.19361917968750075,-0.8721757406249965
2420.849,13.36499999999985,0.8515625,0.078125,0.484375,0.3329576296874897,0.19737808593750072,-0.8488705218749968
2435.933,15.083999999999875,-0.765625,0.0390625,0.71484375,0.2913823546874901,0.1994992734375007,-0.8100527906249971
2453.358,17.425000000000246,1.37890625,0.14453125,-0.26171875,0.37788114374999127,0.20856571875000082,-0.8264704078124974
2471.017,17.658999999999647,-0.078125,0.078125,0.46484375,0.37291454999999135,0.2135323125000007,-0.796919174999998
2488.319,17.302000000000373,-0.46875,-0.078125,0.23828125,0.3437174249999907,0.20866612500000062,-0.7820773031249977
2498.355,10.035999999999934,0.0078125,0.0078125,0.49609375,0.3439996874999907,0.2089483875000006,-0.7641536343749977
2504.933,6.577999999999751,1.5703125,0.06640625,0.03515625,0.38118594374998926,0.21052094062500054,-0.7633211062499978
2520.651,15.71800000000012,-0.60546875,0.06640625,0.484375,0.346925615624989,0.21427852500000055,-0.7359128437499975
2540.7039999999997,20.052999999999876,-0.8359375,-0.01171875,0.390625,0.2865786187499894,0.21343253906250054,-0.7077133124999978
2600.744,60.04000000000032,-1.21875,0.078125,0.6015625,0.023153118749987996,0.2303187890625006,-0.5776891874999971
2700.391,99.64700000000005,-1.29296875,0.01171875,0.24609375,-0.4406725265625122,0.2345226468750006,-0.48940817343749704
2708.0009999999997,7.609999999999673,-0.01171875,-0.01953125,0.46875,-0.44099357343751217,0.23398756875000062,-0.4765662984374976
2735.22,27.219000000000104,0.2578125,-0.0859375,0.6328125,-0.4157309390625121,0.2255666906250006,-0.41455801406249737
2750.3669999999997,15.1469999999998,0.640625,-0.09765625,0.046875,-0.3807981703125125,0.2202415734375007,-0.4120019578124974
2757.812,7.445000000000146,-1.51171875,0.02734375,0.671875,-0.42131525625001337,0.22097444062500068,-0.39399436406249705
2768.011,10.19900000000007,1.83984375,0.0859375,0.48046875,-0.3537628171875129,0.22412975625000073,-0.37635328124999695
2775.443,7.432000000000105,0.2890625,-0.25,0.23828125,-0.3460288921875128,0.21744095625000062,-0.36997801874999686
2782.983,7.540000000000102,-1.3984375,-0.01171875,0.5390625,-0.3839880796875133,0.21712286250000062,-0.3553457062499966
2792.8269999999998,9.843999999999742,0.98828125,-0.11328125,0.453125,-0.3489649734375142,0.21310835625000074,-0.33928768124999703
2803.283,10.45600000000002,-0.09375,-0.05859375,0.01171875,-0.3524938734375142,0.21090279375000073,-0.338846568749997
2817.648,14.365000000000183,1.07421875,-0.1328125,0.9140625,-0.29694172500001353,0.2040345281250006,-0.29157674062499644
I am trying to obtain an estimated speed from the IMU data stream of an OAK-D-POE camera. The basic math is simple: velocity = acceleration/dt, in theory, is the average velocity of the camera (on a specific axis) over the time interval dt relative to the previous period dt.
If acceleration is negative, the speed in the interval dt will be negative and vice versa.
Thus, the velocity relative to the ground is the sum of the relative speeds.
Obviously, this approach can produce errors derived from inaccurate data produced by the IMU, and so filters and corrections must be introduced, such as setting the speed to zero when there is no lateral or vertical acceleration, which indicates that the camera is stationary.
However, from the tests I have done, I get absolutely incorrect data.
Has anyone tried and found a solution?
Hi Team !
I need to find smart mounting solution to fix my OAK-D-POE camera using RAM-MOUNT tools but I can't figure out which is the correct hole mounting stardard used un the back of the camera.
Unfortunatelly I can't use the tripod mounting hole in the bottom side.
Thanks, Stefano
Hi guys!
I'm looking for a developer for a UI application showing a simple alert panel.
Alert comes from the camera that have been programmed to recongnize person within a perimeter.
A beta camera fw has already been developed, so we need the developer to finalize it and build a UI.
Plese contact me at: stefano.dellavalle@itway.com