- Edited
Hi @DiproChakraborty .
I suppose that you downloaded the source code of the app and tried to start it locally? Right?
It does not work this way with Luxonis Hub (LH). Those applications are working inside the LH only.
So you need a device (it can be anything running supported OS - like RasPi 4 or 5) with connected OAK camera. Then you can maintain the device and it's apps from your Mac via web browser.
- Create your account on LH and log in.
- Connect your device and follow the instructions. It will install the agent to the device. Its a service that provides a communication between the device and the LH.
Please note, you need direct SSH access to the device for setup.
Access the device list in the left-hand panel. Locate your newly configured device and open its details page. Navigate to the "App" tab, where you can install the apps from the list.