edxian I'm not sure of the temperature at the minute to be honest but noticed it getting warm when I was only previewing video and thought it worth planning ahead. Mine is in an enclosure with a fan at the back and two vents the other side of the 3P board, I'm expecting air passing it will be enough from the size of the heatsink so haven't looked at putting a fan on it directly.
edxian

- Oct 2, 2023
- Joined Sep 11, 2023
- 0 best answers