D
dcuccia

  • Jul 31, 2023
  • Joined Mar 23, 2023
  • 0 best answers
  • Hi dcuccia ,
    It should work from the sensor perspective, but since it's not specifically for OAK, it likely means no one actually tried it (at least from our team). That said, it should work, but I can't say for 100%. And if it would work, I don't think you'd need the adapter - as arducam ffc cables are directly compatible with OAK, whereas RPi cables are a bit wider so you need the UC244 adapter to be compatible.

  • Hi dcuccia ,
    Luxonis uses Arducam as the only camera supplier, so it would be from Arducam anyways🙂 So it would perhaps be best to check up with them on it.
    Thanks, Erik