Bboseul
- Jul 27, 2022
- Joined Jun 28, 2022
- 0 best answers
erik Thank you
However, I already tried that docs but my depthai doesn't have createToF(), even createCamera() so I changed the code to createColorCamera(). May I know which version of depthai has these functions? And the documentation tells me to checkout the 'branch', but I don't know how to do it. As mentioned above, install_requirements.py has already been run.Hello, I am using OAK-FFC-pToF and OAK-FFC-IMX477-M12 (Arducam) connected to OAK-FFC-3P. I connected Arducam to CAM_C and tof camera to CAM_L. I tried to run cam_test.py of depthai-python for testing, but an error occurred. After running install_requirements.py in depthai-python/examples, I ran cam_test.py. But the below error occurred.
(tof) D:\boseul\depthai-python-tof_rgb_mono\tests>python cam_test.py -cams rgb,c left,t
Enabled cameras:
rgb : color
left : tof
DepthAI version: 2.17.1.0
DepthAI path: C:\Users\HERO\AppData\Roaming\Python\Python39\site-packages\depthai.cp39-win_amd64.pyd
Traceback (most recent call last):
File "D:\boseul\depthai-python-tof_rgb_mono\tests\cam_test.py", line 151, in <module>
tof[c] = pipeline.createToF()
AttributeError: 'depthai.Pipeline' object has no attribute 'createToF'How can I download the depthai library with createToF?
- Edited
Hi, I currently use OAK-D-IOT-40 and want to run standalone mode. I ran various bootloader examples, but dai.DeviceBootloader.getFirstAvailableDevice() is executed. However, if the information resulting from this function is executed as an input to the dai.DeviceBootloader() function, the operation stops. No error message is displayed and the terminal just hangs.
And I tried running the 'device manager.py' in depthai-python, it finds the model name of the device, but when I click the model name, the 'device manager' UI stops. How can I solve this? All I want is to run standalone mode with OAK-D-IOT-40.