B
bitterisland6

  • Jun 16, 2023
  • Joined May 19, 2023
  • 1 best answer
  • Hi guys, sorry to insist but I am still unable to use the two FFC-6P I ordered.

    I had actually installed the luxonisos-1.11 (the latest available version) so I tried to install the luxonisos-1.9 version to match @bitterisland6 's configuration. It is still not detected, and now I can't ssh into the board anymore :/

    I tried the older and newer ips without success

    On the other 6P board we have, I haven't updated anything, I am able to ssh into it, and I noticed errors in the file ~/hddl_logs/hddl_device_service_0.log.last`

    Any thoughts ?

    Thanks !

    • erik replied to this.
    • @bitterisland6 This is due to the resolution set (default 1080p), please set it explicitly for now with -cres 800.
      (We'll have to fix the default handling, or error out.)