A
actebay

  • Joined Jan 12, 2021
  • 0 best answers
  • Images from right and left cameras. The image from the left camera has a softer focus than the image from the right camera. Looking at the depth images they are noisier than I was expecting, for example compared with depth images from my Intel Realsense r200 camera, and was wondering if the softer focus would impact the quality of the depth images.


    • I have just received an OAK-D and I have noticed that the left mono camera is not as well focused as the right mono camera. Is it possible to manually adjust the focus of the mono cameras? If so are there instructions anywhere on your web site for adjusting this?
      Thanks.
      Andy Tebay