T
Thingymagig

  • Jan 16, 2021
  • Joined Jan 12, 2021
  • 0 best answers
  • Brandon

    Hi,

    Took me a few days to get back to my computer for this.

    I'm running Windows 10 Pro N on an AMD Ryzen 7 3700X with 32GB of RAM using git bash for my shell (as powershell really sucks).

    The versions of python, etc. are:

    $ python --version
    Python 3.8.2
    
    $ pip --version
    pip 20.3.3 from c:\python38\lib\site-packages\pip (python 3.8)
    
    $ python -m pip install -r requirements.txt
    Looking in indexes: https://pypi.org/simple, https://artifacts.luxonis.com/artifactory/luxonis-python-snapshot-local/
    Ignoring opencv-python: markers 'platform_machine == "armv7l"' don't match your environment
    Requirement already satisfied: opencv-python==4.2.0.34 in c:\python38\lib\site-packages (from -r requirements.txt (line 1)) (4.2.0.34)
    Requirement already satisfied: depthai==0.0.2.1+b9918c481abaaeac51dd1d2b80fe6a150612f90a in c:\python38\lib\site-packages (from -r requirements.txt (line 4)) (0.0.2.1+b9918c481abaaeac51dd1d2b80fe6a150612f90a)
    Requirement already satisfied: numpy>=1.17.3 in c:\python38\lib\site-packages (from opencv-python==4.2.0.34->-r requirements.txt (line 1)) (1.19.3

    The version of the codebase I was testing was https://github.com/luxonis/depthai-experiments/commit/7cfbd821f65fda1613de90579a030e8ac77eff39

    Let me know if there's anything else I can provide on this and I promise I'll be slightly quicker in responding next time 🙂

    Thanks,

    Nick

    • Hi,

      I got my OAK-1 and OAK-D today and started testing. I'm getting an issue with the pedestrian-reidentification demo through in that within about 5 - 60 seconds of it starting it always crashes with the following:

      Traceback (most recent call last):
        File "main.py", line 132, in <module>
          nn_data.setLayer("data", to_planar(det_frame, (48, 96)))
        File "main.py", line 28, in to_planar
          return [val for channel in cv2.resize(arr, shape).transpose(2, 0, 1) for y_col in channel for val in y_col]
      cv2.error: OpenCV(4.2.0) C:\projects\opencv-python\opencv\modules\imgproc\src\resize.cpp:4045: error: (-215:Assertion failed) !ssize.empty() in function 'cv::resize'

      Any ideas?

      Thanks!