R
ReemOthman

  • Oct 26, 2023
  • Joined Sep 11, 2023
  • 0 best answers
  • @ReemOthman we used ethernet over usb rather than WiFi. Based on our experience if you're using Linux check the firewall isn't blocking the connection as this was one problem we had. Secondly if you are on the newest firmware we had to set the address manually and then revert to DHCP to get it to connect properly on occassion (also on Linux). For some reason the connection seems to work better on windows a lot of the time.