Appreciate the response.
When I try with 2022.3 I get this exception when running mo command. However 2023.1 no issues.
[ ERROR ] Exception occurred during running replacer "REPLACEMENT_ID" (<class 'openvino.tools.mo.load.tf.loader.TFLoader'>): Unexpected exception happened during extracting attributes for node StatefulPartitionedCall/Postprocessor/BatchMultiClassNonMaxSuppression/Slice_3/begin.
Original exception message: index -1 is out of bounds for axis 0 with size 0
"The support for MyriadX was deprecated in 2023 OpenVINO versions" Does that mean I can't use models optimized with openvino 2023.1 with any OKA-D devices?
Is there any other way to generate MyriadX blob format for these devices since 2022 versions not working? any suggestions?