I have not turned it on yet since I cut the bottom label/plate. I'm just assuming it changes, but it may not be noticeable.
Next time I turn it on I'll post an update.
Wwintermute
- Sep 12, 2024
- Joined Oct 15, 2023
- 0 best answers
8mm horizontal, 7mm vertical.
I managed to open my RAE by cutting the edges of the label/bottom plate to expose the screws.
One note is that below the label it's the same translucent plastic as the border/edges (which the LEDs shine through) so cutting the bottom label will change the way the LEDs glow on the floor and that may not be desirable (it's quite simple to mask it out again but just bringing it up).
RAE construction seems pretty solid:
- screws are screwed on the metal case, so you should be able to open/close RAE many times without any issues (just don't over-tighten the screws as it's aluminium).
- wires inside are well attached and not hanging aroundI had RAE running around my house a little bit and it grabbed a lot of hair/dust on the wheels, so opening RAE may be a necessary maintenance step.
- Edited
Yep, that's a good idea! I'll draw a cutting template to share.
The label seems to be quite thick, I think it would be quite destructive indeed.
I see! I really wonder what's the reasoning to make the screws that inaccessible.
I guess with some heat I'll be able to unglue this plate to expose the screws.Thank you!
Hello!
First of all, I'd like to say that I love this project and all the work put into it. It's amazing!
I got my RAE on Friday, and I'd like to ask - how should I proceed to open my RAE to have access to the PCBs, etc?
I couldn't find any instruction and there are no screws visible. Is the enclosure glued?Thank you!