V
victorlu

  • Apr 20, 2022
  • Joined Mar 23, 2022
  • 0 best answers
  • Hi,
    I have read this post. I'm interested to know if RGBD point clouds will be supported in the future release. My project needs the color information of point clouds to feed into YOLO. It would be great to know the timeframe you are about to add this feature.
    Thanks,
    Victor


  • erik Now I'm trying to set up my OAK-D camera without a router because I don't have access to it when I'm outside.

    My thought is to connect the OAK-D camera to my machine through a PoE splitter. My machine will work as a gateway to communicate with the camera. I would like to know if you have any tutorials for that setup.

    • erik replied to this.
    • Thank you erik,

      I have solved this issue by myself. I must set the PoE camera IP address next to my machine's IP address though they are in the same subnetwork by the previous setting (netmask 255.255.255.0). For example, the PoE camera should have 192.168.50.80 when my machine uses 192.168.50.83. But I cannot explain the reason behind it. I hope this will help someone who encounters the same error

    • Hello, I have been struggling with this error for a while and cannot get any progress 😅

      I followed this OAK PoE devices setup tutorial. My machines uses 192.168.50.83 and OaK-D camera uses 192.168.50.8. They are in the same range I believe. These address are setup by the DHCP of router. I can ping camera address under the same LAN. Besides, I can see the occasionally flash so it won't be a power issue.

      I tried to turn off the ufw but I got the sample script just freezing which I needed to terminate forcefully. I have no idea how to troubleshoot now in this case. It would be helpful if anyone has an idea about this error.

      • erik replied to this.