T
tekt

  • Nov 10, 2022
  • Joined Dec 16, 2021
  • 0 best answers
  • erik I've tried to change the IP settings on the device, but device_manager is unable to connect to it. It seems to be able to query its state and configuration, but when I try to flash the configuration, it fails (see below).

    I don't currently have physical access to the device, but it's starting to seem like that might be necessary to fix this, with a direct usb connection as described here:
    https://docs.luxonis.com/projects/api/en/latest/components/bootloader/#boot-switches

    The error:
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 264; Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 373; Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 243; 'NoneType' object has no attribute 'isEmbeddedVersion'
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 279; Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 373; Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 243; 'NoneType' object has no attribute 'isEmbeddedVersion'
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 373; Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 344; 'NoneType' object has no attribute 'getType'
    Exception in C:\chhs\depthai-python\utilities\device_manager.py, line 243; 'NoneType' object has no attribute 'isEmbeddedVersion'

  • erik I'm now only seeing each device once, and they're showing some sort of hex ids instead of ips.
    But it's still unable to connect to one of them.

    [0] 18443010D129BF0800 [X_LINK_BOOTLOADER]
    [1] 18443010C1E60D0900 [X_LINK_BOOTLOADER]
    [2] 184430100155000900 [X_LINK_BOOTLOADER]
    File "C:\chhs\depthai\depthai_demo.py", line 670, in run
    self.instance.run_all(self.conf)
    File "C:\chhs\depthai\depthai_demo.py", line 131, in run_all
    self.setup(conf)
    File "C:\chhs\depthai\depthai_demo.py", line 212, in setup
    self._device = dai.Device(self._pm.pipeline.getOpenVINOVersion(), self._deviceInfo, usb2Mode=self._conf.args.usbSpeed == "usb2")
    RuntimeError: Failed to connect to device, error message: X_LINK_DEVICE_NOT_FOUND

    • I have a network with 3 OAK D PoE devices and a server. When I use depthai_demo.py, it shows output like:

      Available devices:
      [0] 192.168.1.4 [X_LINK_BOOTLOADER]
      [1] 192.168.1.3 [X_LINK_BOOTLOADER]
      [2] 192.168.1.2 [X_LINK_BOOTLOADER]
      [3] 192.168.1.3 [X_LINK_BOOTLOADER]
      [4] 192.168.1.2 [X_LINK_BOOTLOADER]
      [5] 192.168.1.4 [X_LINK_BOOTLOADER]

      It seems odd that some of the devices are showing up multiple times.

      I'm able to connect to two of those devices by IP (*.3 and .4), but connections fail to the third one (.2). It produces errors like this:

      File "C:\chhs\depthai\depthai_demo.py", line 560, in run
      self.instance.run_all(self.conf)
      File "C:\chhs\depthai\depthai_demo.py", line 62, in run_all
      self.setup(conf)
      File "C:\chhs\depthai\depthai_demo.py", line 135, in setup
      self._device = dai.Device(self._pm.pipeline.getOpenVINOVersion(), self._deviceInfo, usb2Mode=self._conf.args.usbSpeed == "usb2")
      Failed to connect to device, error message: X_LINK_COMMUNICATION_NOT_OPEN

      Anyone have any ideas how to fix it?

      • erik replied to this.
      • As part of a long-term art installation, I'm using 3 OAK-D PoE devices to track the positions of people standing in front of it.

        My current approach is based on the spatial object tracker with RGB example (with mobilenet ssd). It seems like objects are often lost but rarely removed. I'm seeing large numbers of LOST statuses (including repetitions for the same id) but they mostly (but not entirely) just stay in that state indefinitely.

        First, is there a better approach for this kind of thing? The data I need is just a distance from the device for each tracked person, with ids attached so I can keep track of how long each person has been within range.

        Second, if object tracker / mobilenet-ssd is the best option, can I configure how long it keeps LOST objects before marked them as REMOVED, and some sort of threshold of when it treats an object as NEW vs switching an existing from LOST to TRACKED?

        • erik replied to this.