Thanks for the feedback, that is good to know. It suggests to me the problem is else where in my code, if the centre crop is automatically set.
Mmcopping
- Jan 25, 2024
- Joined May 8, 2023
- 0 best answers
Thank you for your response.
I see that setSensorCrop() requires the top left x and y coordinates of the box. In order to calculate this, i need to know the resolution of the camera (which i set to THE_4_K) and also the original resolution prior to any internal cropping. This is the piece I am not sure how to retrieve.
When I look at getIspSize() or getResolutionSize(), both return (3840, 2160) i.e. THE_4_K. In the case of the oak 1 max, is there a way to see that the initial resolution is (4056, 3040) which is then cropped to (3840, 2160).
For example, in the case of the oak 1 i believe this should return (3840, 2160), indicating i do not need to setSensorCrop(). In the case of the oak 1max this should return (4056, 3040) i.e. the resolution from THE_12_MP, which then allows me to correctly calculate the coordinates for setSensorCrop() for a resolution of (3840, 2160).
In general i always want the centre of my image to align with the centre of the camera, so it would be nice if I can write a function which always ensures this, even if i swap between cameras and/or resolutions.
thanks again.
- Edited
I have a project which sometimes uses an OAK 1 camera and sometimes uses an OAK 1 max camera. For consistency with the imaging I want to use THE_4_K resolution in both instances. However, when I use the OAK 1 max with the 4 K resolution i note that the centre of the image does not align with the centre of the camera, when I switch to the 4000x3000 resolution this is resolved. I would expect the centre point of my image to be the same regardless of the resolution.
My question is: how do i use an OAK 1 max camera with the 4 K resolution, so that the centre of the image does line up with the centre of the camera?
Whatever fix i use must only impact the way the OAK 1 max works and not the OAK 1.
Any help would be great, thanks.