marlu

  • Nov 25, 2024
  • Joined Apr 17, 2023
  • 0 best answers
  • Hi @marlu
    No, the sensor FPS is capped to 60.

    marlu OAK-1 OV9782 is the only version offering this option

    Any device that uses IMX378 usually also has the OV9782 variant available.

    Thanks,
    Jaka

  • Hi @marlu ,
    calibrate.py should improve calibration compared to old calibration approach, but will still fall short to the current rail calibration approach. Perhaps ask on support@Luxonis.com if you could send in your device to our EU office (Ljubljana/Prague) to get your camera recalibrated with the new rail calibration approach.
    Thanks, Erik

  • @marlu @erik do you have any updates on the Multi-Camera Calibration of cameras not facing the same view?
    And did you find a way to undistort the image? i tried to use OAK-D-W POE, faceing the same issue with wrong vectors with calibration. (i´m using the depthai-experiments/gen2-multiple-devices examples)