- Edited
vital If the vis window is up I just hit Q, but if it is outputting to stdout it just keeps looping forever
I hover the mouse cursor over the CV display window and hit 'q' to stop the python program.
vital If the vis window is up I just hit Q, but if it is outputting to stdout it just keeps looping forever
I hover the mouse cursor over the CV display window and hit 'q' to stop the python program.
I'm learning to use the Oak-D Lite, and have it running on the Pi Zero W. I'm wondering about the asymmetric shadow in the depth field. See the screen capture below, in which the camera is looking directly at me (natural lighting from a large window).
I understand that object pixels not visible to both cameras cannot be assigned a depth value, and would expect symmetric shadows to result. Is the pronounced shadow on the right side due to this effect, or something else?