Luxonis-Alex Has this soft sync mechanism for multiple devices connected to the same host been implemented? Both of your ideas sound great. Or can we implement this ourselves, using script nodes or some other lower level access?
Note that I have tried using FSYNC for this purpose, but failed to get the FSYNC example to work: I adapted Luxonis OAK camera trigger FSYNC pin via Script node for DM9098 board (OAK-D S2/Pro/W/Pro W) (github.com) to OAK-1 (disabling left/right) and get the message [184430100113480E00] [1.1.4] [2.306] [Script(7)] [warning] Trigger successful
- but then no frame is received. This could be an error caused by my adaptation attempt, … or is the FSYNC pin even functional on OAK-1?
Any help would be greatly appreciated because I otherwise have to give up my expensive experiment and resort to PTP-synced industrial vision cameras.