H
hjpark

  • May 24, 2023
  • Joined May 22, 2023
  • 0 best answers
  • Solution:

    Use DHCP to fetch an IP from the RVC3 device rather than using a static IP (`169.254.0.10` netmask `255.255.0.0` or `192.168.197.10` netmask `255.255.255.0`) after upgrading the OS as the subnet changes to `255.255.255.240`

    CC: @abroekhof @hjpark erik