- Edited
erik Thanks!
Done. Here is the issue link: luxonis/depthai-core869
erik Thanks!
Done. Here is the issue link: luxonis/depthai-core869
Hi. I am trying to capture images at 15 fps with HDR enabled using the OAK-1-MAX camera. Specifically, I am using the depthai-python/utilities/cam_test.py
script as suggested in this page.
There are two issues:
misc hdr-exposure-ratio=4 hdr-local-tone-weight=75
, I can only capture a maximum of 3 fps.Any help getting me to to 15 fps HDR images is highly appreciated.
Thanks in advance