D
dror-haor

  • Mar 10, 2022
  • Joined Feb 4, 2022
  • 0 best answers
  • Hi erik , I also tried replacing the switch and to add also a router, but didn't work.
    I tried doing the resetting procedure as in the link you added, and still - the device is not found. I got this error message after running the script in your link:

    Traceback (most recent call last):
    with dai.DeviceBootloader(device_info, allowFlashingBootloader=True) as bootloader:
    RuntimeError: Failed to find device (ma2480), error message: X_LINK_DEVICE_NOT_FOUND

    Any other advice here?
    I want to stress that the second camera is preat much a critical part of our system and we can't work without it.
    Dror

    • erik replied to this.
    • Hi erik , after a while that I tried everything I can , i think that something is wrong with the unit. I connected it to the router straight (or through the switch) and none of the devices can "see" the camera. I can't use the script because I can't find the camera and even ping it. From the other hand, I have another oak-d camera that I got in the same shipment, which work perfectly fine.

      What are the options here?

      • erik replied to this.
      • Hi erik , I can't even discover the devices.
        When I run depthai.Device.getAllAvailableDevices() I get empty array...
        How can I specify a statis IP in this case?

        • erik replied to this.
        • Hi Support,I bought two units of the Oak-D-POE.Also bought the Acroid LS6700G-8P 120W POE switch (should be able to deliver up to 30W per output)
          I just got them yesterday and connected them to my windows PC, and IT WORK AMAZING! the image looked very good, and I was able to use the depth ai python api and sdk.
          I left the switch OFF for the night.This morning, I tried to repeat the things I did yesterday, and the units didn't work. The api can't recognize them, and nothing I did helped:Connect/disconnect both units/ the switch (also from the wall outlet)Replacing cablesTesting for connectivity issues (on windows)
          By using IPCONFIG, I find the switch, but nothing else.The units shows constant led light (and once in a while a blink)
          I understand that there are other issues like this online, but none of the solutions there solved my issue.
          I really need your help solving this problem

          Thanks
          Dror

          • erik replied to this.