I'm on windows. How do i check if device is connectable? My camera is new, cable is new and it happens on different computers.
camuser

- Sep 23, 2024
- Joined Sep 1, 2024
- 0 best answers
- Edited
I have a small program which tries to connect to the camera, then takes a frame, then disconnects and then does it again. In 10-30 connections, it crashes, because dai.Device.getAllAvailableDevices() returns empty array. Here is the program:
Here is the output:
open 1
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 2
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 3
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 4
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 5
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 6
Opened Luxonis camera device
got frame (2160, 3840, 3)
Deleted device
open 7
[2024-09-01 03:40:11.610] [depthai] [warning] skipping X_LINK_BOOTED device having name "2.1"
AssertionError: No connected Luxonis cameras, or all of them are in use
Why does it fail to reconnect? Is that hardware bug? How can it be fixed?