- Edited
The enclosure for the OAK-D-Iot looks great!
I have an OAK-D_Iot 75 sitting unused in the box here so I will be keen to buy one of those cases when they become available.
The OAK-D-POE-CM4 sounds awesome. Any rough idea when those may be available to purchase?
I hope that you do make the follow-on with the M12 connector and active illumination. Since USB is not very practical for industrial applications (due to cable length restrictions). I found the current depth perception on non-textured surfaces was not good enough to use for my use case unfortunately. Could I ask the part numbers for the laser / LED illumination components. I would like to look up the specs on the datasheets to anticipate what it may be capable of (if possible).