Ssshesh
- Feb 4, 2022
- Joined Feb 1, 2022
- 0 best answers
- Edited
Recently I moved to Python 3.10.2 and tried running the install_requirements.py that comes with depthai. I see some problem with wheel which I'm not able to resolve. Any help is much appreciated.
Snapshot (partial) of the error dump on my Ubuntu 18.04 LTS. ---------------------------------------------------------------------------------- error: Command "gcc -pthread -Wno-unused-result -Wsign-compare -DNDEBUG -g -fwrapv -O3 -Wall -fPIC -DNPY_INTERNAL_BUILD=1 -DHAVE_NPY_CONFIG_H=1 -D_FILE_OFFSET_BITS=64 -D_LARGEFILE_SOURCE=1 -D_LARGEFILE64_SOURCE=1 -Ibuild/src.linux-x86_64-3.10/numpy/core/src/umath -Ibuild/src.linux-x86_64-3.10/numpy/core/src/npymath -Ibuild/src.linux-x86_64-3.10/numpy/core/src/common -Inumpy/core/include -Ibuild/src.linux-x86_64-3.10/numpy/core/include/numpy -Inumpy/core/src/common -Inumpy/core/src -Inumpy/core -Inumpy/core/src/npymath -Inumpy/core/src/multiarray -Inumpy/core/src/umath -Inumpy/core/src/npysort -I/home/sheshs/Downloads/Beaver1804/Tools/py-venv/opencv-env/include -I/usr/local/include/python3.10 -Ibuild/src.linux-x86_64-3.10/numpy/core/src/common -Ibuild/src.linux-x86_64-3.10/numpy/core/src/npymath -c build/src.linux-x86_64-3.10/numpy/core/src/multiarray/scalartypes.c -o build/temp.linux-x86_64-3.10/build/src.linux-x86_64-3.10/numpy/core/src/multiarray/scalartypes.o -MMD -MF build/temp.linux-x86_64-3.10/build/src.linux-x86_64-3.10/numpy/core/src/multiarray/scalartypes.o.d -std=c99" failed with exit status 1 [end of output]
note: This error originates from a subprocess, and is likely not a problem with pip. ERROR: Failed building wheel for numpy Failed to build numpy ERROR: Could not build wheels for numpy, which is required to install pyproject.toml-based projects [end of output]
note: This error originates from a subprocess, and is likely not a problem with pip. error: subprocess-exited-with-error × pip subprocess to install build dependencies did not run successfully. │ exit code: 1 ╰─> See above for output. note: This error originates from a subprocess, and is likely not a problem with pip. Traceback (most recent call last):