nikosgavalakis

  • Jun 10, 2023
  • Joined May 14, 2023
  • 0 best answers
  • Hi, I am a student at the university of the aegean(design engineer department) and we are running a project, building an autonomous vessel. We have the oak-d pro camera but I find it hard running a custom tflite model that I trained on it. I want to deploy the model and get as output the distance, position and type of object using the built in depth function of the camera module. The documentation on how to deploy a model seems vague at best and I have the added problem that I have only managed to create a tf lite model instead of tensorflow model which can be converted to .blob. It would be a shame to not use such a capable module. Any help or guidance would be greatly appreciated!!!