J
jonas

  • Oct 14, 2022
  • Joined Jul 27, 2022
  • 0 best answers
  • Thanks erik... I've actually managed to run everything with native modules, including the gen2-experiments and the depthai-demo application. Even Qt does its job.

    The tricky part is to have the correct version of depthai-sdk. The official demo and most of the gen2-experiments work if I directly install the version from the current depthai git repo. You must not run the install requirements scripts, because they usually reinstall stuff you don't want. I've just installed the missing dependencies manually.

    Thus, I'm currently very happy and looking forward to develop my own stuff. Thanks for everything so far!

  • Hi all, I've just received my OAK-D Pro and I'm wondering whats now the "gold standard" to run DepthAI (Python) on a Silicon-based Mac? Is it the approach discussed here or is there now a "Out-of-the-Box"-approach for DepthAI-SDK?

    I did this and was able to run the rgb_preview script. How do I then install the depthai-sdk and run the demo_script?

    • erik replied to this.