garymok

  • Oct 30, 2023
  • Joined Sep 11, 2023
  • 0 best answers
  • erik

    I have followed the example but encountered when building the docker image (on my Mac M1). I have to update the "--platform" parameter of docker build command to "linux/arm64" instead of "arm64". Otherwise, it will prompt error "failed to solve: no match for platform in manifest".

    And then, the docker build process get stuck at step #7 with error as below:

    Sometimes, the error is:

    WARNING: experimental flag squash is removed with BuildKit. You should squash inside build using a multi-stage Dockerfile for efficiency.

    [+] Building 38.4s (10/16) docker:desktop-linux

    [+] Building 340.5s (11/16) docker:desktop-linux

    => [internal] load .dockerignore 0.0s

    => => transferring context: 2B 0.0s

    => [internal] load build definition from Dockerfile 0.0s

    => => transferring dockerfile: 1.49kB 0.0s

    => [internal] load metadata for docker.io/luxonis/depthai-ros-rae:latest 2.1s

    => [ 1/12] FROM docker.io/luxonis/depthai-ros-rae@sha256:5ac6773187d4564a28deed1e013b52a8349583dc8abfeea83220029bca278130 0.0s

    => => resolve docker.io/luxonis/depthai-ros-rae@sha256:5ac6773187d4564a28deed1e013b52a8349583dc8abfeea83220029bca278130 0.0s

    => [internal] load build context 0.0s

    => => transferring context: 12.77kB 0.0s

    => CACHED [ 2/12] RUN apt-get update && apt-get -y install --no-install-recommends software-properties-common git libusb-1.0-0-dev wget zsh python3-colcon-common-extensions python3-rosdep build-essen 0.0s

    => CACHED [ 3/12] RUN mkdir -p /ws/src 0.0s

    => CACHED [ 4/12] COPY ./ ./ws/src/rae-ros 0.0s

    => CACHED [ 5/12] RUN rm -rf ./ws/src/rae-ros/rae_gazebo 0.0s

    => CACHED [ 6/12] RUN cd ./ws/ && apt update && rosdep update && rosdep install --from-paths src --ignore-src -y --skip-keys depthai --skip-keys depthai_bridge --skip-keys depthai_ros_driver --skip-ke 0.0s

    => ERROR [ 7/12] RUN cd ./ws/ && . /opt/ros/humble/setup.sh && . /depthai_ws/install/setup.sh && colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=RelWithDebInfo 338.2s

    ------

    [ 7/12] RUN cd ./ws/ && . /opt/ros/humble/setup.sh && . /depthai_ws/install/setup.sh && colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=RelWithDebInfo:

    1.279 Starting >>> rae_msgs

    1.291 Starting >>> rae_bringup

    1.294 Starting >>> rae_camera

    1.298 Starting >>> rae_description

    2.296 Finished <<< rae_description [1.00s]

    2.563 Finished <<< rae_bringup [1.27s]

    4.855 Finished <<< rae_msgs [3.58s]

    4.855 Starting >>> rae_hw

    316.3 --- stderr: rae_camera

    316.3 CMake Warning (dev) at CMakeLists.txt:67 (add_executable):

    316.3 Policy CMP0115 is not set: Source file extensions must be explicit. Run

    316.3 "cmake --help-policy CMP0115" for policy details. Use the cmake_policy

    316.3 command to set the policy and suppress this warning.

    316.3

    316.3 File:

    316.3

    316.3 /ws/src/rae-ros/rae_camera/src/perception_ipc_rtabmap.cpp

    316.3 This warning is for project developers. Use -Wno-dev to suppress it.

    316.3

    316.3 c++: fatal error: Killed signal terminated program cc1plus

    316.3 compilation terminated.

    316.3 gmake[2]: *** [CMakeFiles/yolo.dir/build.make:76: CMakeFiles/yolo.dir/src/yolo.cpp.o] Error 1

    316.3 gmake[1]: *** [CMakeFiles/Makefile2:232: CMakeFiles/yolo.dir/all] Error 2

    316.3 gmake[1]: *** Waiting for unfinished jobs....

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_pair.cpp: In function ‘int main()’:

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_pair.cpp:23:28: warning: ‘void dai::node::ColorCamera::setColorOrder(dai::ColorCameraProperties::ColorOrder)’ is deprecated: Use 'setPreviewType()' instead [-Wdeprecated-declarations]

    316.3 23 | monoLeft->setColorOrder(dai::ColorCameraProperties::ColorOrder::BGR);

    316.3 | ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

    316.3 In file included from /usr/local/include/depthai/pipeline/nodes.hpp:6,

    316.3 from /usr/local/include/depthai/depthai.hpp:17,

    316.3 from /ws/src/rae-ros/rae_camera/src/stereo_pair.cpp:4:

    316.3 /usr/local/include/depthai/pipeline/node/ColorCamera.hpp:140:59: note: declared here

    316.3 140 | [[deprecated("Use 'setPreviewType()' instead")]] void setColorOrder(ColorCameraProperties::ColorOrder colorOrder);

    316.3 | ~~~~~~~~~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp: In function ‘int main()’:

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:36:59: warning: ‘dai::CameraBoardSocket::LEFT’ is deprecated [-Wdeprecated-declarations]

    316.3 36 | monoLeftFront->setBoardSocket(dai::CameraBoardSocket::LEFT);

    316.3 | ~~~

    316.3 In file included from /usr/local/include/depthai/device/CalibrationHandler.hpp:5,

    316.3 from /usr/local/include/depthai/depthai.hpp:9,

    316.3 from /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:4:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:25:5: note: declared here

    316.3 25 | LEFT [[deprecated]] = CAM_B,

    316.3 | ~~~

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:36:59: warning: ‘dai::CameraBoardSocket::LEFT’ is deprecated [-Wdeprecated-declarations]

    316.3 36 | monoLeftFront->setBoardSocket(dai::CameraBoardSocket::LEFT);

    316.3 | ~~~

    316.3 In file included from /usr/local/include/depthai/device/CalibrationHandler.hpp:5,

    316.3 from /usr/local/include/depthai/depthai.hpp:9,

    316.3 from /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:4:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:25:5: note: declared here

    316.3 25 | LEFT [[deprecated]] = CAM_B,

    316.3 | ~~~

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:38:60: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 38 | monoRightFront->setBoardSocket(dai::CameraBoardSocket::RIGHT);

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/device/CalibrationHandler.hpp:5,

    316.3 from /usr/local/include/depthai/depthai.hpp:9,

    316.3 from /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:4:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:38:60: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 38 | monoRightFront->setBoardSocket(dai::CameraBoardSocket::RIGHT);

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/device/CalibrationHandler.hpp:5,

    316.3 from /usr/local/include/depthai/depthai.hpp:9,

    316.3 from /ws/src/rae-ros/rae_camera/src/stereo_depth.cpp:4:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp: In function ‘dai:😛ipeline createPipeline(bool, bool)’:

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:29:56: warning: ‘dai::CameraBoardSocket::RGB’ is deprecated [-Wdeprecated-declarations]

    316.3 29 | camRgb->setBoardSocket(dai::CameraBoardSocket::RGB);

    316.3 | ~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:23:5: note: declared here

    316.3 23 | RGB [[deprecated]] = CAM_A,

    316.3 | ~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:29:56: warning: ‘dai::CameraBoardSocket::RGB’ is deprecated [-Wdeprecated-declarations]

    316.3 29 | camRgb->setBoardSocket(dai::CameraBoardSocket::RGB);

    316.3 | ~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:23:5: note: declared here

    316.3 23 | RGB [[deprecated]] = CAM_A,

    316.3 | ~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:30:30: warning: ‘void dai::node::ColorCamera::setColorOrder(dai::ColorCameraProperties::ColorOrder)’ is deprecated: Use 'setPreviewType()' instead [-Wdeprecated-declarations]

    316.3 30 | camRgb->setColorOrder(dai::ColorCameraProperties::ColorOrder::BGR);

    316.3 | ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

    316.3 In file included from /ws/src/rae-ros/rae_camera/src/camera.cpp:15:

    316.3 /usr/local/include/depthai/pipeline/node/ColorCamera.hpp:140:59: note: declared here

    316.3 140 | [[deprecated("Use 'setPreviewType()' instead")]] void setColorOrder(ColorCameraProperties::ColorOrder colorOrder);

    316.3 | ~~~~~~~~~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:31:31: warning: ‘void dai::node::ColorCamera::setInterleaved(bool)’ is deprecated: Use 'setPreviewType()' instead [-Wdeprecated-declarations]

    316.3 31 | camRgb->setInterleaved(false);

    316.3 | ~~~~~~~~~~~~~~~~~~~~~~~~~~~~

    316.3 In file included from /ws/src/rae-ros/rae_camera/src/camera.cpp:15:

    316.3 /usr/local/include/depthai/pipeline/node/ColorCamera.hpp:146:59: note: declared here

    316.3 146 | [[deprecated("Use 'setPreviewType()' instead")]] void setInterleaved(bool interleaved);

    316.3 | ~~~~~~~~~~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:58:55: warning: ‘dai::CameraBoardSocket::LEFT’ is deprecated [-Wdeprecated-declarations]

    316.3 58 | leftFront->setBoardSocket(dai::CameraBoardSocket::LEFT);

    316.3 | ~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:25:5: note: declared here

    316.3 25 | LEFT [[deprecated]] = CAM_B,

    316.3 | ~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:58:55: warning: ‘dai::CameraBoardSocket::LEFT’ is deprecated [-Wdeprecated-declarations]

    316.3 58 | leftFront->setBoardSocket(dai::CameraBoardSocket::LEFT);

    316.3 | ~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:25:5: note: declared here

    316.3 25 | LEFT [[deprecated]] = CAM_B,

    316.3 | ~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:60:56: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 60 | rightFront->setBoardSocket(dai::CameraBoardSocket::RIGHT);

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:60:56: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 60 | rightFront->setBoardSocket(dai::CameraBoardSocket::RIGHT);

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp: In function ‘int main(int, char**)’:

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:198:135: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 198 | sensor_msgs::msg::CameraInfo rgbCameraInfo = rgbConverter.calibrationToCameraInfo(calibrationHandler, dai::CameraBoardSocket::RIGHT, width, height);;

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 /ws/src/rae-ros/rae_camera/src/camera.cpp:198:135: warning: ‘dai::CameraBoardSocket::RIGHT’ is deprecated [-Wdeprecated-declarations]

    316.3 198 | sensor_msgs::msg::CameraInfo rgbCameraInfo = rgbConverter.calibrationToCameraInfo(calibrationHandler, dai::CameraBoardSocket::RIGHT, width, height);;

    316.3 | ~~~~

    316.3 In file included from /usr/local/include/depthai/common/CameraBoardSocket.hpp:5,

    316.3 from /usr/local/include/depthai/device/DeviceBase.hpp:18,

    316.3 from /usr/local/include/depthai/device/Device.hpp:14,

    316.3 from /ws/src/rae-ros/rae_camera/src/camera.cpp:13:

    316.3 /usr/local/include/depthai-shared/common/CameraBoardSocket.hpp:26:5: note: declared here

    316.3 26 | RIGHT [[deprecated]] = CAM_C,

    316.3 | ~~~~

    316.3 c++: fatal error: Killed signal terminated program cc1plus

    316.3 compilation terminated.

    316.3 gmake[2]: *** [CMakeFiles/stereo_pair.dir/build.make:76: CMakeFiles/stereo_pair.dir/src/stereo_pair.cpp.o] Error 1

    316.3 gmake[1]: *** [CMakeFiles/Makefile2:258: CMakeFiles/stereo_pair.dir/all] Error 2

    316.3 gmake: *** [Makefile:146: all] Error 2

    316.3 ---

    316.3 Failed <<< rae_camera [5min 15s, exited with code 2]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 [Processing: rae_camera, rae_hw]

    337.7 Aborted <<< rae_hw [5min 33s]

    337.9

    337.9 Summary: 3 packages finished [5min 37s]

    337.9 1 package failed: rae_camera

    337.9 1 package aborted: rae_hw

    337.9 2 packages had stderr output: rae_camera rae_hw

    ------

    Dockerfile:19

    --------------------

    17 | RUN cd .$WS/ && apt update && rosdep update && rosdep install --from-paths src --ignore-src -y --skip-keys depthai --skip-keys depthai_bridge --skip-keys depthai_ros_driver --skip-keys audio_msgs --skip-keys laserscan_kinect --skip-keys ira_laser_tools

    18 |

    19 | >>> RUN cd .$WS/ && . /opt/ros/${ROS_DISTRO}/setup.sh && . $UNDERLAY_WS/install/setup.sh && colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=${BUILD_TYPE}

    20 |

    21 | RUN echo "if [ -f ${WS}/install/setup.zsh ]; then source ${WS}/install/setup.zsh; fi" >> $HOME/.zshrc

    --------------------

    ERROR: failed to solve: process "/bin/sh -c cd .$WS/ && . /opt/ros/${ROS_DISTRO}/setup.sh && . $UNDERLAY_WS/install/setup.sh && colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=${BUILD_TYPE}" did not complete successfully: exit code: 2

    • I have just received my RAE. However, is there any example codes, for e.g., how to control LED, motors, etc.? Also, kickstarter campaign page mentioned that there will be mobile APP available for controlling it. When will it be available?

      • erik replied to this.
      • I have just received my RAE. However, is there any example codes, for e.g., how to control LED, motors, etc.? Also, kickstarter campaign page mentioned that there will be mobile APP available for controlling it. When will it be available?

        • erik replied to this.