F
fredrikq

  • Apr 24, 2022
  • Joined Apr 19, 2022
  • 0 best answers
  • Just tested the sample code and it works like a charm!

    By the way, I got the following error message after a while:

    [184430102110111300] [387.892] [system] [critical] Temperature above 105C. Device will shutdown if not reduced. Note: If this is unexpected please reach out to support@luxonis.com to discuss/debug.

    OAK-D Lite camera is connected thru a USB cable.

    Any idea why this happens?

    Thanks!

    • Hi!
      I am just a newbie here and would like to detect persons(any model) by using OAK-D Lite camera on Windows 10 and then display distance as well.

      Is there any "simple" code that I can refer to?

      Regards,
      Fred.

      • erik replied to this.