eraydoan

- Jan 8, 2024
- Joined Nov 30, 2023
- 0 best answers
- Edited
Hi,
I want to make object traking system. I'm using just OAK-D camera and S7-1200 PLC. I will define imaginary line on the cam. If the object pass the line , camera will give data/logic 1 to PLC . How can i make it?
Thanks,
Hi,
I want to make object traking system. I'm using just OAK-D camera and S7-1200 PLC. I will define imaginary line on the cam. If the object pass the line , camera will give data/logic 1 to PLC . How can i make it?
thanks,