E
eimarinb

  • Mar 21, 2022
  • Joined Mar 10, 2022
  • 0 best answers
  • This is not the answer.. compile the wheel for the M1 is the solution:

    whab — 01/22/2022
    For those struggling with running DepthAI natively on their M1 computers, here are step-by-step instructions to build, install and test a M1 native version of DepthAI in less than 30 minutes (tested on a new MacBookPro M1 Pro running macOS Monterey 12.1 with a OAK-D-Lite):

    # Install native M1 version of brew
    /bin/bash -c "$(curl -fsSL https://raw.githubusercontent.com/Homebrew/install/master/install.sh)"
    echo 'eval "$(/opt/homebrew/bin/brew shellenv)"' >> ~/.zprofile
    eval "$(/opt/homebrew/bin/brew shellenv)"
    
    # Install conda to create virtual environments for Python
    brew install --cask miniconda
    conda init zsh
    Close and re-open a Terminal window
    
    # Install DepthAI by building a M1 wheel (inside ~/DepthAI/)
    conda create --name DepthAIEnv39 python=3.9
    conda activate DepthAIEnv39
    python3 -m pip install -U pip
    brew update
    brew install cmake libusb
    cd ~; mkdir DepthAI; cd DepthAI
    git clone --recursive  https://github.com/luxonis/depthai-python.git
    cd depthai-python
    mkdir build && cd build
    cmake ..
    cmake --build . --parallel
    cd ..
    python3 -m pip wheel . -w wheelhouse
    pip install wheelhouse/depthai-*
    
    # Test DepthAI with a OAK plugged to your new M1 Mac
    cd examples
    nano install_requirements.py
        Remove code of block (3 lines) starting with: if thisPlatform == "arm64" and platform.system() == "Darwin":
        Remove code of block (48 lines) starting with: if not args.skip_depthai:
    python3 install_requirements.py
    python3 ColorCamera/rgb_preview.py

    Enjoy!