D
dschroeder

  • May 14, 2024
  • Joined Oct 18, 2023
  • 0 best answers
  • Thanks @alex_007! I'm pretty inexperienced with c++, but I think I get the gist. Using the HDevEngine over creating a framegrabber certainly makes sense.

  • Hey @jakaskerl thanks for the reply.

    When used in UVC mode, I'm guessing it only uses one of the camera inputs instead of both? Can 3d vision still be gotten through UVC?

    • Does anyone know if the Oak-D Pro PoE (or any of the Oak cameras) would be compatible with MVTec Halcon?

      Halcon does support the following interfaces:

      • GenICam
      • GigE Vision
      • USB3 Vision
      • CoaXPress
      • Camera Link

      It's possible I'm just blind, but I'm having difficulty finding specifics about the OAK-D communication standards.