D
dandiode

  • Aug 16, 2024
  • Joined Sep 16, 2023
  • 0 best answers
  • Ive been having trouble getting the Rae to connect ever since I received it. Initially it took a lot of effort to get it to connect to wifi and the firmware update kept stalling.
    I tried again to get it going a couple of days later but now its not responding at all. last time I tried to shut it down it appeared to hang in the shutdown mode and didnt respond to anything so I let it run the battery down to shut off.

    After recharging it powered up and displayed RAE on the screen but nothing further, totally unresponsive, so I shut it down. that worked ok. Powering up again, the same response, so I used the factory reset button. This brought it back to the RAE start screen but again now it hangs in shutdown and not responsive to anything. What is going on? Seems like there is something going badly wrong in the firmware

    • Hey
      Ive just got the RAE and it doesnt log in to wifi well at all. It took several attempts to get the initial login/signup working, even with the device right next to the wifi router (about 30cm away) - everything else in the house gets the wifi ok (all other connected devices apart from this computer were off while attempting setup).

      Now it is logged in ok but the updates dont appear to work properly. The loading seems to progress but when it looks to be finished it just hangs and a message "Upgrade is taking longer than usual" appears on the screen. Its in the screenshot below:
      Also, live mode doesnt work, it just displays "Waiting for a stream" and then hangs. Again with the rae right next to the router and everything else off. Is there something Im missing here? Is there an option to do the updates over USB?