Sagar

  • Mar 20, 2023
  • Joined Mar 15, 2023
  • 0 best answers
  • I have an OAK-D S2 POE camera. I have connected it to my private network via the LAN cable. I access the camera through the network as my PC is also connected to the same network. When I access the camera using the Windows OS, I get disconnected from the internet after 10 minutes. I can ping other devices in the same network but I can't use the internet anymore. Also, other PCs connected to the same network can't ping me. If I restart the PC then I am connected to internet again. However, this doesn't happen when I use Ubuntu OS. Does anyone have any idea as to why this would happen?