Hi @Robert ,
Sorry I missed this somehow!
Q1: Can a fixture be glued to the bottom of the above enclosure (perhaps a smaller enclosure) and the following be used to mount the OAK-D as-is with current Aluminum Housing? See this url,
?
Yes, I do think that would work.
Q2. In Regards to Power, is there any reason these 2 components could not be used to supply power to OAK-D,
(a) Portable 1200 mAh UPS Lithium Battery Power Module for Raspberry Pi, Connected to...
(b) Female 5.5x2.1mm to Male 4.0x1.7mm, 3.5x1.35mm, 3.0x1.1mm, 2.5x0.7mm Jack, USB to DC 5.5x2.1mm Cord (DC4+1) ?
Yes, I think that should work. Note that OAK-D can also be powered by any device that can provide USB3 power (900mA). So potentially you could just power OAK-D via USB only w/out the external power adapter.
More info is here: https://docs.luxonis.com/en/latest/pages/faq/#can-i-power-depthai-completely-from-usb
Sorry again about missing this... not sure how I did.
-Brandon