Hello! I've been experimenting with my new OAK-4-S with depthai-3 but I'm having trouble setting the brightness and focus manually. I've following the following examples but unfortunately I can't understand this bit
RexMello

- 21 days ago
- Joined Nov 28, 2023
- 0 best answers
In OS Update I need to ssh into the device IP. On the guide it says I don't need a password. However when I try doing ssh into the camera, it asks for a password. I tried "luxonis", "admin" and "root" and get permission denied error
root@10.0.10.93's password:
Permission denied, please try again.
root@10.0.10.93's password:
I tried with sudo permission too but that doesn't help either. What should I do?
The issue we're facing currently is that all oakctl commands give that failed to wait for response error. I'll try reconnecting it or with USB and update the OS. After reconnecting it works sometimes
Thanks for reaching out, I tried that and also
oakctl device info
Both commands give me an error saying
"Comms error: Failed to wait for response"Could the error be in hardware?
I recently got an OAK-4-S and its been running fine. Sometimes however the issue I face time to time is that my camera stops working and when I try to run OAK-Viewer I get an error saying device is already in use while none of my code is running. I tried restarting the PC but that doesn't help so I replug the camera and that fixes it most of the time. Any help would be appreciated
Ushavilash Sorry but I'm not sure how it's done. Can you point me at some article or anything that shows it? Thanks!
- Edited
Thanks @jakaskerl ! I read that and it had link to
https://docs.luxonis.com/projects/api/en/latest/samples/Camera/camera_undistort/#undistort-camera-streamThat helped me undistort most of the curved issue. However it doesn't let me set resolution to more thatn 1920x1080, is there a way to use full 4k?
Greetings! I recently bought an OAK-D and an OAK-1 camera and I'm still learning about their features. In the demo scripts provided on github my OAK-D camera gives me sort of like a curved view. Is it because of the wide angle? Is there a way to disable that? I want to fetch a flat view