Q
QuantumNature

  • Sep 10, 2024
  • Joined Feb 22, 2024
  • 0 best answers
  • Hello,

    To preface, these aren't huge concerns as no functional damage has yet been done and I intend/hope to eventually use external motors to move Rae, so this feedback is mainly in hopes it may be useful to the development and improvement of the product 💝

    First, upon opening Rae, I noticed that the front LED bar ribbon cable is being cut into by the hall sensor of one of the motors. The LED bar still works, and there is no functional damage yet, but I haven't used it much and in time I imagine it may cut through more and kill the front lights. A bit of extra tape would help 🙂

    Second, the motors often don't fully stop when input is stopped (via the default app); they'll keep spinning slowly for a while, usually one motor more than the other. Video example: https://photos.app.goo.gl/VkEM6poE7E1p4SuSA

    Third, the motors aren't of equal strength or spin at different rates, so straight forward is rarely actually straight, and turning is not an in-place spin. The two motors also have very different sounds, with one motor sounding like it is struggling. Video example: https://photos.app.goo.gl/5n9KrExhRz6xRGiA8

    Again, these issues aren't huge for my use case, but hopefully they could be improved in the future.

    Let me know if I can provide any more information that could be of use.

  • Robot was definitely online. And team ID? Team name is "Pink", is that what you need to ID my Rae?

    • On RobotHub I see there is an update to the 'Agent Version', but whenever I click the up arrow button to "Upgrade Agent to latest version" it hangs in 'Upgrading from 23.223.1855 to 24.031.1223 / Waiting for device to connect...'. Is this currently expected?

      I'm not sure if related, but I do see this in the log file /var/log/daemon.log:

      2024-03-03T21:50:17.187984+00:00 rae hddl_device_service[567]: #033[1;31;40m[21:50:17.1867][567]ERROR[XLinkPlatform.cpp:88] devices_num = 1, no pcie device found, retry after 2 seconds ...#033[0m
      2024-03-03T21:50:17.220529+00:00 rae robothub-tunnel.mjs[577]: {"component":null,"context":{},"level":20,"logger":{"config":{"format":"json","level":10,"rootComponent":"tunnel","runtime":"production"},"name":"tunnel"},"message":"killing process by pid 4212 (read from /run/user/1001/rh-ttyd.pid)","when":"2024-03-03T21:50:17.219Z"}
      2024-03-03T21:50:17.220848+00:00 rae robothub-tunnel.mjs[577]: {"component":null,"context":{"error":{"code":"ESRCH","errno":-3,"message":"kill ESRCH","name":"Error","stack":"Error: kill ESRCH\n    at process.kill (node:internal/process/per_thread:233:13)\n    at killProcessByPidFile (file:///usr/libexec/robothub/robothub-tunnel.mjs:42119:15)\n    at file:///usr/libexec/robothub/robothub-tunnel.mjs:42217:9\n    at file:///usr/libexec/robothub/robothub-tunnel.mjs:31253:16","syscall":"kill"}},"level":40,"logger":{"config":{"format":"json","level":10,"rootComponent":"tunnel","runtime":"production"},"name":"tunnel"},"message":"kill 4212 failed","when":"2024-03-03T21:50:17.219Z"}
      2024-03-03T21:50:17.222818+00:00 rae robothub-tunnel.mjs[577]: {"component":null,"context":{"args":["--interface","/home/robothub/ttyd.sock","--socket-owner","robothub:robothub","-cwd","/home/robothub","--debug","15","-t","enableZmodem=true","-t","enableTrzsz=true","-t","enableSixel=true","-t","disableLeaveAlert=true","-t","disableResizeOverlay=true","-t","fontSize=15","-t","theme={\"background\": \"#111\"}","bash"],"bin":"/usr/libexec/robothub/ttyd"},"level":30,"logger":{"config":{"format":"json","level":10,"rootComponent":"tunnel","runtime":"production"},"name":"tunnel"},"message":"starting 'ttyd'","when":"2024-03-03T21:50:17.221Z"}
      2024-03-03T21:50:17.231342+00:00 rae robothub-tunnel.mjs[577]: {"component":null,"context":{},"level":30,"logger":{"config":{"format":"json","level":10,"rootComponent":"tunnel","runtime":"production"},"name":"tunnel"},"message":"'ttyd' started with PID 4216","when":"2024-03-03T21:50:17.230Z"}
      2024-03-03T21:50:17.233331+00:00 rae robothub-tunnel.mjs[4216]: ttyd: invalid credential, format: username:password
      2024-03-03T21:50:17.234627+00:00 rae robothub-tunnel.mjs[577]: {"component":null,"context":{"exitCode":255,"signal":null},"level":30,"logger":{"config":{"format":"json","level":10,"rootComponent":"tunnel","runtime":"production"},"name":"tunnel"},"message":"ttyd exited","when":"2024-03-03T21:50:17.233Z"}
      2024-03-03T21:50:19.188682+00:00 rae hddl_device_service[567]: #033[1;31;40m[21:50:19.1873][567]ERROR[XLinkPlatform.cpp:88] devices_num = 1, no pcie device found, retry after 2 seconds ...#033[0m

      This error occurs regardless of which app runs (though, I have yet to get any app to work other than the default app)

      When clicking update, robothub-ctl logs says:

      ...
      level=info msg="Loaded configuration file: /var/lib/mender/mender.conf" module=config
      level=warning msg="No server URL(s) specified in mender configuration." module=config
      level=warning msg="Server entry 1 has no associated server URL." module=config
      level=info msg="Mender running on partition: /dev/mmcblk1p8" module=main
      level=info msg="Performing remote update from: [https://luxonisos.fra1.digitaloceanspaces.com/build/1.14-rae+6263cb8c60f2cbfc80cc523f2b37581eb38139aa/luxonisos-1.14-rae.dm-verity.mender]." module=standalone
      level=info msg="no public key was provided for authenticating the artifact" module=installer
      level=info msg="Update module output: Updating rootfs: /dev/mmcblk1p5" module=modules
      ... minutes later ...
      level=info msg="Update module output: Updating rootfs: /dev/mmcblk1p6" module=modules
      level=error msg="Download connection broken: stream error: stream ID 1; NO_ERROR" module=update_resumer
      level=info msg="Resuming download in 1m0s" module=update_resumer
      ... a little later ...
      level=info msg="Attempting to resume artifact download from offset 867356933" module=update_resumer
      63 22:01:55  I  root/agent/root : firmware upgrade> upgrade was successful, rebooting after 5 seconds
      {
        "code": 0
      }
      ... rae reboots, on reconnect ...
      63 22:03:04  I  user/agent : user: robothub
      63 22:03:04  I  user/agent/hub/config : startup cloud state
      {
        "connectionConfig": {
          "remoteHost": "robothub.luxonis.com",
          "remoteProto": "ssl",
          "remoteWebPort": null
        },
        "decodedToken": null,
        "team": null,
        "token": "present",
        "webUri": "https://robothub.luxonis.com"
      }
      63 22:03:05  W  user/agent/local-mqtt : cant connect to mqtt, is broker running?
      63 22:03:06  W  user/agent/local-mqtt : cant connect to mqtt, is broker running?
      63 22:03:06  E  user/agent/apps : failed to kill container b8028d63c54efbbed09dc0d71d7ea6ebc58ce2d85f9f27dc6a020c7230f2cec9: Error: killContainer exited with 125
      63 22:03:06  I  agent/nanomq : starting nanomq process...
      63 22:03:06  I  user/agent/hub-connection : no longer calling home (waiting if token removed)
      63 22:03:06  I  user/agent/hub-connection : MQTT connection -> connecting... wss://gateway.robothub.luxonis.com
      Sun, 03 Mar 2024 22:03:06 GMT body-parser deprecated undefined extended: provide extended option at node:internal/process/task_queues:60:5
      63 22:03:06  I  user/agent/http-server : HTTP Server listening on 127.0.0.1:9009
      63 22:03:06  I  user/agent/http-server : HTTP Server listening on 0.0.0.0:9010
      63 22:03:06  I  agent/nanomq : NanoMQ Broker is started successfully!
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [805] ERROR /home/runner/work/nanomq/nanomq/nng/src/sp/protocol/mqtt/auth_http.c:281 send_request: Connect failed: Connection refused
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [805] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/protocol/mqtt/nmq_mqtt.c:728 nano_pipe_start: Invalid auth info.
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [805] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:610 tcptran_pipe_recv_cb: nni aio recv error!! Object closed
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [805] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:872 tcptran_pipe_recv_cb: tcptran_pipe_recv_cb: recv error rv: 139
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [808] ERROR /home/runner/work/nanomq/nanomq/nng/src/sp/protocol/mqtt/auth_http.c:281 send_request: Connect failed: Connection refused
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [808] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/protocol/mqtt/nmq_mqtt.c:728 nano_pipe_start: Invalid auth info.
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [808] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:610 tcptran_pipe_recv_cb: nni aio recv error!! Object closed
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq : 2024-03-03 22:03:06 [808] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:872 tcptran_pipe_recv_cb: tcptran_pipe_recv_cb: recv error rv: 139
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  I  agent/nanomq :
      63 22:03:06  W  user/agent/hub-connection : network error (connection-refused) | address: undefined
      63 22:03:06  E  root/agent/root : mqtt error
      {
        "error": {
          "code": 135,
          "message": "Connection refused: Not authorized",
          "name": "Error",
          "stack": "Error: Connection refused: Not authorized\n    at MqttClient._handleConnack (file:///usr/libexec/robothub/robothub-agent.mjs:38517:21)\n    at MqttClient._handlePacket (file:///usr/libexec/robothub/robothub-agent.mjs:37916:16)\n    at work (file:///usr/libexec/robothub/robothub-agent.mjs:37822:16)\n    at writable._write (file:///usr/libexec/robothub/robothub-agent.mjs:37837:9)\n    at doWrite (file:///usr/libexec/robothub/robothub-agent.mjs:27194:16)\n    at writeOrBuffer (file:///usr/libexec/robothub/robothub-agent.mjs:27179:9)\n    at Writable.write (file:///usr/libexec/robothub/robothub-agent.mjs:27101:15)\n    at Socket.ondata (node:internal/streams/readable:766:22)\n    at Socket.emit (node:events:513:28)\n    at Socket.emit (node:domain:489:12)"
        }
      }
      63 22:03:07  I  user/agent/apps : local sync (db -> containers) - assigning devices to apps...
      63 22:03:07  I  user/agent/apps : local sync (db -> containers) - assigning orphan devices to builtin apps...
      {
        "device": [
          "3C52A016838860C5"
        ]
      }
      63 22:03:07  I  user/agent/apps : local sync (db -> containers) - assigning orphan devices to builtin apps...
      {
        "device": [
          "3C52A016838860C5"
        ]
      }
      63 22:03:07  I  stream-handler : PID: 818
      63 22:03:07  I  stream-handler : loading bootstrap configuration from "/etc/robothub-agent/agent.toml"
      63 22:03:07  I  user/agent/apps : local sync (db -> containers) | storedApps = 1 | containers = 1
      63 22:03:07  I  user/agent/apps : local sync (db -> containers) - ensure stored containers...
      63 22:03:07  I  stream-handler/rtc-connection : configured
      63 22:03:08  I  user/agent/apps : expected app[117fc4de-c8c9-4361-895f-1a43be8f1eed] to be running, but its stopped -> starting...
      63 22:03:09  I  agent/nanomq : 2024-03-03 22:03:09 [805] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:610 tcptran_pipe_recv_cb: nni aio recv error!! Connection shutdown
      63 22:03:09  I  agent/nanomq :
      63 22:03:09  I  agent/nanomq : 2024-03-03 22:03:09 [805] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:872 tcptran_pipe_recv_cb: tcptran_pipe_recv_cb: recv error rv: 139
      63 22:03:09  I  agent/nanomq :
      63 22:03:09  I  agent/nanomq :
      63 22:03:11  I  agent/nanomq : 2024-03-03 22:03:11 [808] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:610 tcptran_pipe_recv_cb: nni aio recv error!! Connection shutdown
      63 22:03:11  I  agent/nanomq :
      63 22:03:11  I  agent/nanomq : 2024-03-03 22:03:11 [808] WARN  /home/runner/work/nanomq/nanomq/nng/src/sp/transport/mqtt/broker_tcp.c:872 tcptran_pipe_recv_cb: tcptran_pipe_recv_cb: recv error rv: 139
      63 22:03:11  I  agent/nanomq :
      63 22:03:11  I  agent/nanomq :
      63 22:03:11  I  user/agent/apps : local sync (db -> containers) - cleanup of old containers...
      63 22:03:11  I  user/agent/apps : local sync (db -> containers) - cleanup of old containers...
      63 22:03:11  I  user/agent/apps : local sync (db -> containers) - done
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner/mqtt-client : subscription-change -> connected, fromConnect = false
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner/mqtt-client : subscribed to app/117fc4de-c8c9-4361-895f-1a43be8f1eed/inner
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner/mqtt-client : subscribed to app/117fc4de-c8c9-4361-895f-1a43be8f1eed/forward
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner/mqtt-client : subscribed to app/117fc4de-c8c9-4361-895f-1a43be8f1eed/+/fe
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner : respawning app
      63 22:03:12  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:12  D  inner/mqtt-client : subscription-change -> connected, fromConnect = false
      63 22:03:13  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:13  I  inner : [2024-03-03 22:03:13.266] [depthai] [warning] USB protocol not available - If running in a container, make sure that the following is set: "-v /dev/bus/usb:/dev/bus/usb --device-cgroup-rule='c 189:* rmw'"
      63 22:03:13  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:13  D  inner : app status changed to: running
      63 22:03:13  I  user/agent/local-mqtt : [117fc4de-c8c9-4361-895f-1a43be8f1eed] -> 63 22:03:13  D  inner/mqtt-client : subscription-change -> connected, fromConnect = true
      63 22:03:16  I  user/agent/hub-connection : MQTT connection -> connecting... wss://gateway.robothub.luxonis.com
      63 22:03:18  W  user/agent/hub-connection : Last agent upgrade probably failed
      63 22:03:24  I  user/agent/hub-connection : received see_you
      63 22:03:24  I  user/agent/hub-connection : Connection with server established, communication enabled!

      The mender command from this post to downloaded the update manually does the same thing.