Prinal

  • 19 Jan
  • Joined 14 Jan
  • 0 best answers
  • Hi Jaka,

    Yeah while running the SpatialOnHostDemo, we kept the ROI entire intact to the object. But still the error range of ~5 inches is showing. Are there any other configuration changes apart from the one you suggested we need to try?

    • Hi Jaka,
      Im using this SpatialOnHostDemo. All Im doing is plugin in the OAK-D Pro, run the demo and see the measurement on the screen from the object (me standing in the front of the camera). Then when I measure the distance from the camera to the me standing at the same position using a measuring tape, Im getting a error range of 5 inches. Which I think is significant when Im standing only 60 inches far from the camera.

      • Thank @jakaskerl. I tried changing the useSpec=True, but that still generated ~5 inches of error like the previous runs. My devices MXID=14442C1011D4D2D600. Thanks for helping on this.

        • Hey guys I just bought the OAK-D PRO. On the factory setting I ran this SpatialOnHostDemo, where I was standing in a straight line from the camera at a distance of 60 inches (1.5 m) where I was getting a error range of 5 inches. Im pretty new to using this camera and the depthai as well. Can someone please help me if I need to change the camera configurations or my approach on getting the depth measure to reduce the error to less than 1 inch. Any suggestions are highly appreciated! 🙂