N
Narender

  • 12 days ago
  • Joined Mar 20, 2024
  • 0 best answers
  • Hello

    got below sometimes in oakdpro

    INFO: Opening OAK-D Pro device

    [MonoCamera(1)] [error] Camera not detected on socket: 1

    [MonoCamera(0)] [error] Camera not detected on socket: 2

    INFO: Opened OAK-D Pro device

    Ran this python script(luxonis/depthai-pythonblob/main/utilities/cam_test.py) and below is the output

    python3 cam_test.py -show

    Enabled cameras:

    rgb : color

    left : mono

    right : mono

    camd : color

    DepthAI version: 2.24.0.0

    DepthAI path: /path

    cam_test.py:320: DeprecationWarning: Use constructor taking 'UsbSpeed' instead

    with dai.Device(*dai_device_args) as device:

    [1944301081559A2E00] [1.3] [0.929] [ColorCamera(9)] [error] Camera not detected on socket: 3

    Connected cameras:

    -socket CAM_A : IMX378 4056 x 3040 focus:auto - COLOR

    -socket CAM_B : OV9282 1280 x 800 focus:fixed - MONO

    -socket CAM_C : OV9282 1280 x 800 focus:fixed - MONO

    USB speed: SUPER

    IR drivers: [('LM3644', 2, 99)]

    Cam: rgb left right camd [host | capture timestamp]

    FPS: 0.00| 0.00 0.00| 0.00 0.00| 0.00 0.00| 0.00

    [right, 0, 6141.393650] Exp: 30.001 ms, ISO: 1549, Lens pos: -1, Color temp: 6500 K

    Ran second time and there was no error

    device restarted after two days and got the same error again.

    can anyone let me know how to resolve this.

    thanks.