MasterBlaster

  • Dec 8, 2023
  • Joined Nov 29, 2023
  • 0 best answers
  • thanks for the reply. I am in a local network that regularly rotates IPS so wanted a way to periodically capture and send images to my pc (with minimal external involvement)

    I was looking into the available libraries for Leon, I can see email, but no smtplib or py-emails. As far as I understand the standard email package does not provide capabilities to send emails.

    Is there a way to send email directly from the camera?

    (If so, I could send its IP via email during every IP rotation and subsequently connect with the device)

    • Hello, i am able to get poe with example mjpg server running, but I need to install a few python packages for my application to run. I have searched but could not find. how do I install say boto on the camera