LeviStrieter

  • Jun 2, 2023
  • Joined Jun 1, 2023
  • 0 best answers
  • I have a pallet of boards, all the same color and different sizes, stacked on top of each other. My camera is directly over the pallet looking down on it, sometimes a smaller board sits on top of a larger board and the neural net will only detect the larger board. Is it possible to use the depth camera to find the board at the highest point and then set the roi to look an inch down from that point (board height is an inch), So I would almost be performing a scan down the pallet layer by layer. Any guidance in the right direction would help.

    Thanks