J
JPRotec

  • May 3, 2024
  • Joined Feb 21, 2024
  • 0 best answers
  • jakaskerl So from my understanding, it can't combine ToF and stereo depth images automatically?
    I will have to combine them myself if I want to?

  • Is it true that the OAK-D SR PoE will have both ToF and stereoscopic 3D capabilities?
    If it has both, can you pick which one to use or will it combine their results into a single depth image?

    My reason for thinking it has both, is because the specifications indicate it has:

    • Time of Flight (ToF) VGA (640x480 @ 30fps)
    • Two OV9782 (1 MP Color Global Shutter)

    And I assumed the two OV9782 would take care of the stereoscopic images.

  • @GustavoVelasquez I don't know what OS you are running on the raspberry, but I'm assuming it's some kind of Unix distribution.

    configPath = Path(r'C:\\Users\\gusta\\Desktop\\depthai-experiments\\gen2-yolo\\device-decoding\\5\\best.json')

    Therefore it probably won't have a C: drive.
    Don't know if that is the problem, but just a suggestion.