GoksanISIL

  • Feb 10, 2024
  • Joined Feb 10, 2024
  • 0 best answers
  • hi! I'm interested in on-the-edge sensor fusion applications on OAK-D. Most of the pipeline examples are communicating to the host. Is there any example where I can see some basic on-device camera-imu sync sort of functionality? I can see that there is scripting mode but I was wondering if there is a clear C++ application where we can configure the RTOS queues etc. I would only like to transmit the end result to host, so no computation on host.

    Thanks!