G
Gianlucaiit

  • Sep 18, 2024
  • Joined Aug 1, 2024
  • 0 best answers
  • Hello everyone, in our lab we are currently testing our OAK-D PRO camera to detect point clouds of cylindrical PVC pipes. However, we have noticed that, keeping a fixed distance from the camera (z-axis of the camera) of about 35 cm, the point clouds become increasingly noisy as we move closer to the bottom-right corner of the camera's field of view. Generally, we could say that the affected area is the triangle with vertices at the bottom-left corner, bottom-right corner, and top-right corner. I am attaching the three point clouds separately, as well as a point cloud with the three overlaid, and two photos of the current setup. The room is moderately lit without any direct light sources pointed at the camera. Any ideas on why this noise is occurring?

    I also opened an issue here: luxonis/depthai-core1085
    Here's the material: user-attachments/files16455011/Luxonis.material.zip