G
GbekeAdesiyun

  • Aug 10, 2023
  • Joined Jun 20, 2023
  • 0 best answers
  • Hi,

    Is the maximum fps for the Oak-1 MAX camera 60? I'm curious because I can see on one Luxonis website that the fps is 60 and on a different Luxonis website the fps is 42. These are screenshots from the two different websites being referred to.

    • Hi,

      Thanks for the quick reply. No, I'm not receiving frames at 60FPS. I believe the host computer can write to the disk fast enough . Okay, I'll use those functions to find out the time consumed and get back to you.

    • Hi, I'm currently working on a vision project using the Oak-1 camera, but I have been unable to get the number of frames saved to be consistent with the fps set (60 fps) in the code even though I used the setFps() function to specify the fps for the project. The max fps for the Oak-1 camera is 60 according to the documentation, so I know the fps is not too large. Any ideas on what can be done to resolve this?

      • erik replied to this.