GK2024

- May 10, 2024
- Joined Feb 12, 2024
- 0 best answers
Hi @GK2024
FPS depends on a number of factors. The model used in detection (the bigger/more complex it is, the slower it will run), size of frames, other processes running in your pipeline.GK2024 in Canada where can i buy the latest OAK-3? how many FPS the OAK-3 support?
I'd honestly wait for the Series 4 if you can. S3 was pulled back a bit because the SOC it was using had a lot of issues. S4 should greatly improve the FPS in most tasks.
Thanks,
JakaHi @GK2024
Checkout examples on how to work with Depthai from inside of RH.- luxonis/robothub-examplestree/main/Working%20with%20low-level%20DepthAI/Object%20Detection%20%2B%20Depth -- detection
- luxonis/robothub-examplestree/main/Applications/Line%20Cross%20Counter -- tracking
Thanks,
Jaka