D
Doo

  • 2 days ago
  • Joined Sep 13, 2023
  • 0 best answers
  • Upgrade your robot's firmware to the latest version (Luxonis OS 1.14). What should I do? Could you explain… .
    Since when did you get rid of the RAE section. I studied LINUX and came in to try to make it work, but it's trying to erase RAE. mmlol . Please upload a site link or show the CLI to update (RAE 1.14).

    • jakaskerl where is the main landing page? I am clumsy on navigation.

    • Knowing that various documents of luxonis had to be reviewed and repaired under Linux, I purchased Raspberry Pi 4, and with difficulty, I flash the image provided by MENDER to the SD card and connected the RAE to USB C. However, I still only see the RAE.

    • Thank you for your helpful reply. Reading the contents, it seems that it is a problem that can be solved only when it is directly connected to RAE.
      1. I'm currently only using Windows pc and it's a work related system, so I think I need to install and start a new OS Linux Ubuntu? Is that right?
      2. Why did the stationary "rae" happen? Is it software? Is it hardware? What should I do to prevent these problems in the future?
      3. Should the expected RAE's controls be programmed directly? As explained in kickstarter, ROS security and hide-and-seek seem to be not something you can do naturally. Then, I think you should provide an app that can be used for the function control you want at any time. Can you promise to do so? (so that it won't be more than $300 scrap metal)

      4. Is Raspberry pi enough to configure the linux system to connect with RAE? Does it work with the Turing Pi (http://turingpi.com ) I recently acquired recently? Is it possible to do Arduino board? (I haven't experienced Linux yet and I'm trying because I want to do it, --I have Raspberry pi/Turing board/Arduino board but I'm not using them ) Please give me some good advice. -
      5 Although there is a little lack of verbal communication in English

      1. I purchased the OAK series that kickstarted from Luxonis, but it was not fully utilized, but I would like to take this opportunity to actively apply it using Linux as Luxonis mentioned. In fact, weekly Webinar is not easy to listen to even if I go in and listen to it (Local time at 2 a.m.), and it would be very helpful to listen to it if you summarize the title and contents before doing the webinar... I would appreciate it if you could tell me the site where I can watch the rerun of the webinar.
      2. What should I do??? Please solve these problems in front of me.
      • erik replied to this.
      • When the robot Rae is switched on, it only shows "rae" on LCD and cannot proceed. If I press the switch twice, it will shutdown. What should I do? Should I send RAE to Luxonis (company)? Teach me how to fix it.

        Before requesting support, please see: https://docs.luxonis.com/en/latest/pages/support/

        • erik replied to this.
        • The LCD of the RAE stops with "rae" and does not proceed any further. What should I do?