CharlesSun

  • Oct 10, 2023
  • Joined Oct 4, 2023
  • 0 best answers
  • I resolved the problem by uninstalling the default app 1.1.0 and then installing 1.1.1

  • I just received my RAE robot and connected to it via Robothub. However, the default app failed to run. Here is the error log:

    2023-10-04 00:33:13 UTC INFO | stop:131 => Shutting down ROS2 context...

    2023-10-04 00:33:13 UTC INFO | _destroy_publishers_and_subscribers:142 => Destroying /battery_status subscriber...

    2023-10-04 00:33:13 UTC INFO | _destroy_publishers_and_subscribers:138 => Destroying /cmd_vel publisher...

    2023-10-04 00:33:13 UTC INFO | stop:125 => Destroying ROS2 node...

    2023-10-04 00:33:13 UTC INFO | _spin:112 => rlcpy thread> Done

    2023-10-04 00:33:13 UTC INFO | on_stop:42 => Stopping the app...

    2023-10-04 00:33:13 UTC

    2023-10-04 00:33:13 UTC IndexError: list index out of range

    2023-10-04 00:33:13 UTC File "<string>", line 82, in init_streams

    2023-10-04 00:33:13 UTC File "<string>", line 39, in on_start

    2023-10-04 00:33:13 UTC self.on_start()

    2023-10-04 00:33:13 UTC File "/lib/robothub/app.py", line 161, in _run

    2023-10-04 00:33:13 UTC Traceback (most recent call last):

    2023-10-04 00:33:13 UTC ERROR | _run:165 => App crashed during initialization

    How can such an obvious problem exist right out of the box for this product?

    Did I miss something?