Adrien

  • May 14, 2023
  • Joined May 14, 2023
  • 0 best answers
  • I'M having trouble with connecting my camera to the depthai_demo.py script or any of my other working scripts. I am on a MAC M2. Everything was working fine just last week so I'm not sure what happened. Let me know if there is anything else I can try, I tried reinstalling dependencies from the depthai repo but that didn't do anything. Here is my error code:

    Using depthai module from:  /Users/adrien/Library/Python/3.10/lib/python/site-packages/depthai.cpython-310-darwin.so
    Depthai version installed:  2.21.2.0
    Setting up demo...
    Available devices:
    [0] 194430102186771300 [X_LINK_UNBOOTED]
    Traceback (most recent call last):
      File "/Users/adrien/Repos/depthai/depthai_demo.py", line 1053, in <module>
        runOpenCv()
      File "/Users/adrien/Repos/depthai/depthai_demo.py", line 1043, in runOpenCv
        demo.run_all(confManager)
      File "/Users/adrien/Repos/depthai/depthai_demo.py", line 132, in run_all
        self.setup(conf)
      File "/Users/adrien/Repos/depthai/depthai_demo.py", line 209, in setup
        self._device = dai.Device(self._pm.pipeline.getOpenVINOVersion(), self._deviceInfo, usb2Mode=self._conf.args.usbSpeed == "usb2")
    RuntimeError: Failed to find device after booting, error message: X_LINK_DEVICE_NOT_FOUND
    Exception ignored in atexit callback: <bound method Demo.stop of <__main__.Demo object at 0x128c75510>>
    Traceback (most recent call last):
      File "/Users/adrien/Repos/depthai/depthai_demo.py", line 336, in stop
        self._pv.closeQueues()
    AttributeError: 'Demo' object has no attribute '_pv'
    Sentry is attempting to send 2 pending error messages
    Waiting up to 2 seconds
    Press Ctrl-C to quit